MCX N947: Simultaneous Implementation of Ethernet and Camera Functions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCX N947: Simultaneous Implementation of Ethernet and Camera Functions

MCX N947: Simultaneous Implementation of Ethernet and Camera Functions

Overview

NXP FRDM-MCXN947 board is a low-cost design and evaluation board based on the MCXN947 device. NXP provides tools and software support for the MCXN947 device, including hardware evaluation boards, software development integrated development environment (IDE), sample applications, and drivers. The board is equipped with Ethernet PHY, and also supports camera modules and NXP's low-cost LCD module PAR-LCD-S035.

Harry_Zhang_0-1757560073724.png

 

In this article, we will explore how to simultaneously implement Ethernet connection transmission and image acquisition using a camera on the MCXN947 board.


Hardware Environment

  • Development Board: FRDM-MCXN947
  • Display: 3.5" TFT LCD (P/N PAR-LCD-S035)
  • Camera: OV7670
  • Network Cable: RJ45

Software Environment

  • IDE: MCUXpresso IDE v11.9.0
  • SDK: MCUXpresso SDK Builder (nxp.com)

Pin Configuration and Multiplexing

When designing circuits, attention must be paid to avoiding pin conflicts, that is, ensuring that the same pin is not configured to perform conflicting functions at different times. When configuring pin functions, it is necessary to consider whether their electrical characteristics (such as voltage range, current drive capability, etc.) meet the requirements of the peripherals. When writing software, it is necessary to consider the support for pin multiplexing in different versions of MCU firmware or library files to ensure software compatibility and stability.

Import the "lwip_examples" -> "lwip_ping_bm" project from the FDRM-MCXN947 SDK, open the board -> pin_mux.c file, and you can see the pin configuration for Ethernet connection as shown in the table below:

Pin Name Pinmux Assignment
P1_4 ALT9 - ENET0_TX_CLK
P1_5 ALT9 - ENET0_TXEN
P1_6 ALT9 - ENET0_TXD0
P1_7 ALT9 - ENET0_TXD1
P1_8 ALT9 - ENET0_TXD2
P1_9 ALT9 - ENET0_TXD3
P1_13 ALT9 - ENET0_RXDV
P1_14 ALT9 - ENET0_RXD0
P1_15 ALT9 - ENET0_RXD1
P1_20 ALT9 - ENET0_MDC
P1_21 ALT9 - ENET0_MDIO
 

Download the schematic of the MCXN947 board from NXP's official website, and find the modules corresponding to Camera and FlexIO LCD, as shown below:

Harry_Zhang_1-1757560397299.png

Harry_Zhang_2-1757560410963.png

 

FlexIO is a flexible input/output (I/O) technology developed by NXP, used to provide high-speed, programmable communication capabilities between microcontrollers (MCU) and external devices. It allows developers to configure the FlexIO module inside the microcontroller to simulate various communication protocols and develop custom protocols.

Note: This LCD only supports 3V I/O voltage, so when configuring all pins on this connector, you must ensure they are all set to 3V3 operation mode.

The following diagram shows the working principle of the SDK example, where the camera collects images and transmits them to the LCD display:

Harry_Zhang_3-1757562668813.png

It can be seen that the LCD module does not have any pin conflicts with the pins required for Ethernet and Camera functions, while the pins required for configuring the Camera module are duplicated with Ethernet. The pin reuse can be found in the datasheet provided on the NXP official website as shown in the following table:

Pin Name

Pinmux Assignment

P0_4

ALT0 - P0_4

P0_5

ALT0 - P0_5

P1_4

ALT7 - SmartDMA_PIO0

P1_5

ALT7 - SmartDMA_PIO1

P1_6

ALT7 - SmartDMA_PIO2

P1_7

ALT7 - SmartDMA_PIO3

P1_10

ALT7 - SmartDMA_PIO6

P1_11

ALT7 - SmartDMA_PIO7

P1_18

Default-PIO-Low

P1_19

Default-PIO-High

P2_2

ALT1 - CLKOUT

P3_2

ALT2 - FC7_P0

P3_3

ALT2 - FC7_P1

P3_4

ALT7 - SmartDMA_PIO4

P3_5

ALT7 - SmartDMA_PIO5


As seen above, pins P1_4, P1_5, P1_6, and P1_7 conflict directly with Ethernet pins. Since Ethernet pins are fixed to the RJ45 PHY, the Camera interface must be reassigned to alternate pins.

From the datasheet, P3_0, P3_1, P3_2, and P3_3 can serve as alternatives. However, P3_2 and P3_3 are already used for I²C. To resolve this, they are reassigned to P3_8 and P3_7 respectively (using kPORT_MuxAlt3).

The updated pin mapping is shown below:

Previous Pin

Current Pin

Pinmux Assignment

P1_4

P3_0

ALT7 - SmartDMA_PIO0

P1_5

P3_1

ALT7 - SmartDMA_PIO1

P1_6

P3_2

ALT7 - SmartDMA_PIO2

P1_7

P3_3

ALT7 - SmartDMA_PIO3

P3_2

P3_8

ALT3 - FC7_P0

P3_3

P3_7

ALT3 - FC7_P1

 

Implementation

The reassigned pins (P3_0, P3_1, P3_7, P3_8) are not exposed on the board’s headers, but the schematic shows that they are connected to test pads TP12, TP31, TP18, and TP16. The camera can be wired to these pads directly.

Harry_Zhang_0-1757564251929.png

 
Pin Name Solder Pad
P3_0 TP12
P3_1 TP31
P3_7 TP18
P3_8 TP16
 

Harry_Zhang_2-1757564416860.png

 

Integrate the smartdma_camera_flexio_mculcd example from display_examples into the lwip_ping_bm project. Merge .c and .h files from board, drivers, component, and source folders. Add these folders to the include path under Project -> Properties -> C/C++ Build -> Settings -> Includes.

Harry_Zhang_3-1757564453620.png

 

After integration, compile and flash the project to the board. The output is shown in the images.

Harry_Zhang_4-1757564465243.png

Harry_Zhang_5-1757564478135.png

 


Conclusion

The Ethernet and Camera functions can be simultaneously implemented on the MCX N947 board. The lwip_ping_bm demo showcases ICMP-based Ping functionality using the lwIP TCP/IP stack. It periodically sends ICMP echo requests to a PC and processes the replies.

The smartdma_camera_flexio_mculcd demo demonstrates how to use SmartDMA to capture image data frame-by-frame from the OV7670 camera and display it on the ST7796S LCD panel via FlexIO.

By reconfiguring and multiplexing pins, simultaneous use of Ethernet and Camera on the MCX N947 is achievable.

 

No ratings
Version history
Last update:
2 weeks ago
Updated by: