Hi,
first of all I was amazed to hear that nxp also provides an extension for VS Code cause that is one of my favorite editors.
So I was trying to import an existing project into the MCUXpresso VS Code Extension.
The existing project uses makefiles (not CMake) as toolchain. The project is integrated into the MCUXpresso IDE v. 11.8 for Eclipse. It uses linked folders.
When trying to import that project into MCUXpresso VS Code, I got an error saying "Error: Invalid MCUXpresso IDE project directory: Cannot read properties of undefined (reading '0')". As I read elsewhere, linked folders are not yet supported so I removed the links and copied the sourcecode. This made the error go away, but the vsc code import wizard got another error saying
"Error: Invalid MCUXpresso IDE project directory: The description of the configuration could not be obtained"
I don't know if its possible to get some more info from vscode about what exactly went wrong.
Might it be due to the fact that the project uses makefiles?
Might it be due to the fact that the project is not using the nxp configTools(pins, clocks, etc) at all? I thought about setting up the nxp configTools in eclipse and later deactivating everything in it because we dont need it. However, I seem to cannot set up nxp configTools in the first place.
I am thankful for any support