Unable to select too chain for imx-9 in vscode (ubuntu)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to select too chain for imx-9 in vscode (ubuntu)

1,019 Views
Robbi
Contributor II

Hi team,

                I had installed vs code in Ubuntu along with MUCxpresso extension and Try to fetch the example to compile and debug them but the error Unable to select tool chain  as shown in attached image.

 

Thanks 

Robbi

0 Kudos
Reply
1 Reply

958 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

Have you happened to see an option "Add toolchain path..."? if so, you can try to add by following the instructions.

From the MCUXpresso-SDK should these toolchain supported, 

Supported Toolchains

All driver examples and most application examples are provided with projects for the following toolchains:

If you try MCUXpresso Installer, then should a toolchain be installed.

Hope these references be helpful for you. Getting Started with MCUXpresso for Visual Studio Code | NXP Semiconductors

MCUXpresso extension configuration

Install Repository · nxp-mcuxpresso/vscode-for-mcux Wiki · GitHub

 

Regards

Harvey

0 Kudos
Reply