Manage components not working on VSCode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Manage components not working on VSCode?

ソリューションへジャンプ
1,770件の閲覧回数
jBahae
Contributor I

Hello everyone,

I'm experiencing an issue with managing SDK components in Visual Studio Code. When I click on "Manage components," nothing happens at all.
I access this feature by right-clicking on the project, then selecting Configure → Manage Components.

I've attached a screenshot showing all the tools I have installed. And as you can see, the SDK has been properly added to my repository.
Is there something I'm missing in my setup? Has anyone else encountered this issue and found a solution?

Any help would be greatly appreciated!

0 件の賞賛
返信
1 解決策
1,677件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jBahae,

I have replicated this issue. Indeed, when trying to manage components from a project that was converted to VS Code using the MCUXpresso IDE Project Converter, it won't work. I believe this is a bug and I already reported it to the VS Code team for their review. In the meantime, I recommend you manage the necessary components using the option in MCUXpresso, before importing the project to VS Code. This seems to be the only current workaround.

Sorry for the inconvenience this may cause.

BR,
Edwin.

元の投稿で解決策を見る

3 返答(返信)
1,758件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jBahae,

The manage component option will prompt a component search on the top search bar of VS Code:

EdwinHz_0-1743800198312.png

It might be slow, but after a while of loading the available components, these should display as such:

EdwinHz_1-1743800229775.png

Do you see the top search bar loading? If so, please be patient as it will take a while to load all of the components.

BR,
Edwin.

0 件の賞賛
返信
1,720件の閲覧回数
jBahae
Contributor I
Thank you for your reply. It works for projects created directly in VSCode - I created a new SDK example following your instructions and it worked as demonstrated.
However, my main project was originally developed in MCUXpresso IDE, and I'm now trying to migrate it to VSCode. Is there a way to make this functionality work for projects that were initially created in MCUXpresso IDE?
0 件の賞賛
返信
1,678件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jBahae,

I have replicated this issue. Indeed, when trying to manage components from a project that was converted to VS Code using the MCUXpresso IDE Project Converter, it won't work. I believe this is a bug and I already reported it to the VS Code team for their review. In the meantime, I recommend you manage the necessary components using the option in MCUXpresso, before importing the project to VS Code. This seems to be the only current workaround.

Sorry for the inconvenience this may cause.

BR,
Edwin.