I need a more clear explanation for this.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need a more clear explanation for this.

ソリューションへジャンプ
2,931件の閲覧回数
SoloTheDog
Contributor I

I try to build and download SDK from SDK builder, but get an error that it isn't a proper sdk file when trying to import. When I unzip it and try to import it as a local directory, once I click import nothing happens.

I tried downloading sdk on mcuxpresso and then pointing it to that file but that didn't work either.

I'm trying to use the FRDM_KL02Z board, with the MKL02Z32xxx4 SDK in vscode. I would really much rather use vscode over mcuxpresso if possible.

 

Can someone walk me through how to get the SDK in, create a new project, and start debugging code?

 

I'm able to import a project, but then I can't see my peripheral regs which I would like to see, and get an error that the SVD file is missing. Spent an hour trying to get that to work also to no avail.

 

Any help please! Thank you!!

0 件の賞賛
返信
1 解決策
2,912件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @SoloTheDog 

Unfortunately VScode only supports SDK2.13 and above at the moment.

Alex_Wang_0-1711361491937.jpeg

 

I'm sorry to inconvenience you.

Hope this helps you.

Best regards, Alex

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,903件の閲覧回数
SoloTheDog
Contributor I

Thank you so much. Haha. Sorry, I wasn't aware. Saves me some time looking around.

0 件の賞賛
返信
2,913件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @SoloTheDog 

Unfortunately VScode only supports SDK2.13 and above at the moment.

Alex_Wang_0-1711361491937.jpeg

 

I'm sorry to inconvenience you.

Hope this helps you.

Best regards, Alex

0 件の賞賛
返信
2,896件の閲覧回数
SoloTheDog
Contributor I

Sorry, but wouldn't these SDKs work? 2.3.1 > 2.1.3

0 件の賞賛
返信
2,876件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @SoloTheDog 

Yes, not supported. SDK version 2.13 or later.

Best regards, Alex

 

0 件の賞賛
返信