I have imported a SDK example project into MCUXpresso for VS COde, but I need to change the MCU package. How do I do this?
Solved! Go to Solution.
Hello @olav
"As long as the ports are the same in the two packages (as they are to my knowledge), it does not matter if the package is set to 100pin QFN of 98pin BGA?"
->> Yes, it doesn't matter.
BR
Alice
I have manually hanged every instance of LPC55S69JBD100_cm33 to LPC55S69JEV98_cm33 in the different json files.
The Projects->myProject->MCU-> Package is however still wrong.
But, does it really matter?
As long as the ports are the same in the two packages (as they are to my knowledge), it does not matter if the package is set to 100pin QFN of 98pin BGA?
Hello @olav
"As long as the ports are the same in the two packages (as they are to my knowledge), it does not matter if the package is set to 100pin QFN of 98pin BGA?"
->> Yes, it doesn't matter.
BR
Alice
Hello @olav
There is no change package function like in MCUXpresso IDE, only can change in code.
BR
Alice