Cannot debug "mbox_data" zephyr sample apps. Failed to launch GDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot debug "mbox_data" zephyr sample apps. Failed to launch GDB

ソリューションへジャンプ
3,259件の閲覧回数
Jorini
Contributor I

Good morning,

I’m starting to run some tests with the FRDM-MCXN947 board and the Visual Studio Code environment using the “MCUXpresso” extension, on a 64-bit Windows 11 system.

So far, I’ve successfully downloaded and run several examples from the “MCUXpresso SDK Repository,” including helloworld, blinky, and mailbox_interrupt (multicore), all of which worked correctly.

I’ve also tested examples from the “Zephyr Repository.” All single-core examples work fine, but I’m having issues with the multicore examples — specifically, they don’t run as expected.

In particular, I’m attaching information from the mbox_data example. It compiles without errors, but when I try to run or debug it, the program fails to execute.

I’m attaching the reports for reference.

0 件の賞賛
返信
1 解決策
2,401件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Jorini 

I tested it again. I believe that the CPU1 doesn't get programmed when just pressing the debug button from VSCode. So my steps are:

1. Flash the CPU1 (remote domain)

Harry_Zhang_0-1754044842338.png

Harry_Zhang_1-1754044853886.png

2. Then I can debug the application:

Harry_Zhang_2-1754044926864.png

Harry_Zhang_3-1754044937989.png

I'm able to replicate this each time. Can you please check again?

BR

Harry

 

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
2,997件の閲覧回数
Jorini
Contributor I

Hi @Harry_Zhang,

Thank you for your response and for forwarding the issue to the Zephyr team.

I just wanted to kindly follow up and ask if there have been any updates regarding the multicore example issue, particularly with the mbox_data example on the FRDM-MCXN947 board.

I appreciate your help and any news you can share.

Best regards,

0 件の賞賛
返信
2,905件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Jorini 

I just tested it. My Zephyr VERSION is 

(VERSION_MAJOR = 4
VERSION_MINOR = 2
PATCHLEVEL = 0
VERSION_TWEAK = 0
EXTRAVERSION = rc3)

Harry_Zhang_0-1752828943987.png

It can work now, you can test it.

BR

Harry

0 件の賞賛
返信
2,829件の閲覧回数
Jorini
Contributor I

Hi @Harry_Zhang ,

The image you have attached is from the "blinky" project, this project has always worked for me.

I opened the thread because I couldn't run the "multicore" type projects, specifically the mbox_data. With Zephyr's latest release, I still can't get the "mbox_data" example to run. Any ideas?

Best regards,

Jorini

0 件の賞賛
返信
2,796件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Jorini 

Sorry,  i updated the SDK used in the zephyr environment to 0.17.2 and it is working now. Can you please try updating and testing again?

BR

Harry

0 件の賞賛
返信
2,709件の閲覧回数
Jorini
Contributor I

Hi @Harry_Zhang ,

I've updated what you told me, and it still behaves the same. I'm attaching a screenshot of the project import and the error message it displays when debugging the project. I'm also attaching the installed versions.

 

 

0 件の賞賛
返信
2,437件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Jorini 

I am so sorry, I am still investigating this issue with the team. If there is any progress, I will update immediately. Thank you for your understanding.

BR

Harry

0 件の賞賛
返信
2,402件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Jorini 

I tested it again. I believe that the CPU1 doesn't get programmed when just pressing the debug button from VSCode. So my steps are:

1. Flash the CPU1 (remote domain)

Harry_Zhang_0-1754044842338.png

Harry_Zhang_1-1754044853886.png

2. Then I can debug the application:

Harry_Zhang_2-1754044926864.png

Harry_Zhang_3-1754044937989.png

I'm able to replicate this each time. Can you please check again?

BR

Harry

 

0 件の賞賛
返信
1,990件の閲覧回数
Jorini
Contributor I

Hi @Harry_Zhang , following the steps indicated works correctly. In other projects, the code is automatically loaded into memory, but in these, I see that it isn't. Thanks for your help.

0 件の賞賛
返信
3,236件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Jorini 

Thanks for your information.

I reproduced this issue.

I have reported it to our Zephyr team.

We will fix it as soon as possible.

BR

Harry

0 件の賞賛
返信