MCUXpresso Training Hub

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Training Hub

讨论

排序依据:
Documentation MCUXpresso Secure Provisioning Tool User Guide (Download)  MCUXpresso Secure Provisioning Tool Release Notes    This training currently covers the following areas: Getting Started with MCUXpresso Secure Provisioning Tool  i.MX RT10xx Secure Boot with PEmicro Production Programming  Secure Boot on the i.MX RT10xx Crossover MCUs  
查看全文
This guide covers: How to launch Config Tools for projects in MCUXpresso for VS Code. How to modify and update code from Config Tools. Note: The warning at 1:43 is due to an older version of Config Tools. Note: The dialogue at 2:13 refers to simultaneously route the Wakeup Unit Peripheral that is not needed for this example.
查看全文
GOAL Learn how to import CMSIS packs into existing projects. In this particular project, CMSIS packs from EmSA will be used alongside the lpcxpresso55s16_mcan_interrupt_transfer example obtained from the LPCXpresso55s16 SDK.   ENVIRONMENT This guide requires MCUXpresso IDE v11.9.1 or latest.   PROCEDURE 1. Import the lpcxpresso55s16_mcan_interrupt_transfer example into the workspace. In this example, SDK drivers, startup and board interface files are readily available. CAN pins are already routed and enabled.     2. Launch Config Tools to configure the clock for the CAN peripheral     3. Configure the clock for the CAN peripheral. I. Set up the main clock so that it is generated from crystal or oscillator, and it is evenly dividable by 40 MHz.   II. Change the PLL configuration an even multiple of 40 MHz   III. Set the CAN divider to get a 40 MHz clock.   4. Update the code.   5. Add Open-CMSIS Packs to the project.   6. Project set-up I. Add the watchdog driver.   II. Exclude the fsl_mcan.c module from the build. A dedicated version is included in the EmSA packs.   III. Add the main.c module from CMSIS template   IV. Exclude or remove the original main source code mcan_interrupt_transfer.c file.   7. Save and build the project.          
查看全文
RTOS DETAILS View The RTOS DETAILS view shows various information about RTOS Tasks/Threads. The view appears in the bottom pane, once a debug session is started, and disappears after debugging ends. The view is independent of the debug probe being used, as it only uses GDB commands to receive information from the target. The supported RTOSes are: FreeRTOS  Zephyr    FreeRTOS Usage The RTOS DETAILS view will display the following for FreeRTOS projects. However, the project must be configured properly. TCB#: Task Control Block.  configUSE_TRACE_FACILITY  needs to be set to 1. Task Name: Name of task.  configMAX_TASK_NAME_LEN  needs to be greater than 1. Task Handle: Address of the task handle. Task State: Current task state. Rows are also colored based on the state. Priority: Task actual priority and task base priority. Stack Usage: Graphical view of current stack usage, peak usage and total size for the task. Hovering over the cell reveals more information about the stack.  configRECORD_STACK_HIGH_ADDRESS  needs to be set to 1. Runtime: Task runtime with percentage value.  configGENERATE_RUN_TIME_STATS  needs to be set to 1. Note: The Runtime view needs a patch to FreeRTOS to access runtime counters. See Erich Styger's blog for explanation and patch.     For the FreeRTOS portion of this article, I'll be working with the frdmrw612_freertos_sem example project obtained from the FRDMRW612 SDK. To configure the settings on this project, open the FreeRTOSConfig_Gen.h file. In the FreeRTOSConfig_Gen.h file, use Ctrl+F to quickly find and set the defines highlighted in red above. Save the file.   Once the settings have been configured, build the example and flash the board. The RTOS DETAILS View is available in the bottom pane. To view the data, suspend the target and the view will detect the RTOS type and read information about the tasks/threads. Every time the target stops (suspended or stepped), the RTOS DETAILS view will refresh with updated information.   RTOS DETAILS view has the following capabilities: Resize columns by dragging their edges. Sort columns by clicking on them. Hover over each cell and header to get more information. Color rows by task/thread state. Display warning icons when missing certain RTOS configurations. The warning icons can be hovered for more help on how to solve the issue.     Zephyr Usage The RTOS DETAILS view will display the following for Zephyr projects. Name: Name of the thread.  CONFIG_THREAD_NAME  needs to be enabled. Handle: Address of the thread handle. Priority: Priority of the thread. State: Current task state. Rows are also colored based on the state. Stack Usage: Graphical view of the stack delta offset, current usage and total size for the thread. Hovering over the cell reveals more information about the stack.  CONFIG_THREAD_STACK_INFO  needs to be enabled.   For the Zephyr portion of this article, I'll be working with the philosophers example project obtained from the Zephyr 4.1.0 SDK. To configure the settings on this project, open the prj.conf file. Add the highlighted items above and save the file.   Next, build the project and flash the board. The RTOS DETAILS view will appear on the bottom pane during a debug session as it did for the FreeRTOS example. Expect the behavior to be similar with only a change in the columns.
查看全文
Overview The MCUXpresso SDK 24.12.00 is fully hosted on GitHub. Users are able to clone the SDK and easily keep up to date with changes. Version control transparency allows users to review commits, tags, diffs, etc.   Source Control The MCUXpresso SDK on GitHub is composed of multiple groups of software distributed among different repositories. The MCUXpresso SDK uses the popular west manifest to specify what software is included. This method of delivering software was inspired by Zephyr. The manifests folder contains the manifest file to initialize and update the west workspace. In the mcuxsdk folder you'll find the MCUXpresso SDK source code, examples, middleware integration and script files. Both of these folders contain a .git directory that contains information to track changes, branches, and history of the project.   Visual Studio Code: CLI To interact with the repo within VS Code through a CLI, open a Terminal. The Terminal can be opened from the menu in the top left of the screen. Alternatively, the Terminal and other monitors are hidden in a bar at the bottom of the screen. Navigate to the bottom of the screen, use the cursor to drag the bar and reveal the Terminal.   Once in the CLI, git commands can be run to track the status of the MCUXpresso SDK repositories.   Visual Studio Code: GUI The command line is useful for many things, however, sometimes a gui might be productive. The source control gui that VS Code provides can be accessed through the menu on the top left of the screen or in the extensions sidebar.   The source control gui in Visual Studio Code contains three sections: Source Control Repositories - These are the repositories that are currently visible to the workspace. Each repository contains a menu that allows the user to pull, push, navigate across branches, etc.     Source Control - This tracks changes made by the user. Here, you will see staged changes, commits, etc. *Note: Contribution to the MCUXpresso SDK is currently not open.     Source Control Graph - This provides a comprehensive overview of the project. The graph shows a representation of commits and their related data. The image below shows the source control graph for the MCUXpresso SDK. Hovering over a commit will show the author, commit date, documentation messages, and the commit ID.       Viewing Changes to source One of the main benefits of hosting the MCUXpresso SDK on GitHub is that enables better project management. Users now have access to the entire MCUXpresso SDK project history. Navigate to the Source Control Graph view and select any entry. Doing so will open the diff view highlighting the changes across the modified files in the commit.          
查看全文
Overview Previously, we covered an overview of Kconfig in this article. We also covered, the process of launching the Kconfig GUI from the CLI. In this article, we will look at the process for launching the Kconfig GUI from MCUXpresso for VS Code.   Process Before we can get started with the Kconfig GUI, we need to import a project into VS Code. For this article let's focus on the freertos_hello example as we did in the Kconfig article for the CLI.   To open the Kconfig GUI, navigate to the PROJECTS view. Right click on the freertos-hello project and select Configure > Open Kconfig GUI Configuration.   The Kconfig GUI should launch, you'll now be able to make changes/selections in the GUI.   For example, you can modify the project to use heap 3 rather than heap 4. After selecting the component, you'll see a brief overview and description of the component.     After completing changes with the Kconfig GUI, click the Save button. If your project requires it, make the changes to code in other parts of your project. To verify that changes made from the Kconfig GUI were applied: navigate to the PROJECTS view, expand the project, expand the Project Files, expand the build configuration, and open the .config file. You can view this file directly in the workspace. Use Ctrl + F to find the components that you modify. The verification step is not required. Users are able to attempt a build as soon as they save their changes in the Kconfig GUI.   
查看全文
MCUXpresso SDK The MCUXpresso SDK has been reengineered to make use of CMake and Kconfig. This article will demonstrate how to use the SDK in VS Code.   *Note: The SDK has switched to CalVer versioning convention. *Note: The SDK will contain previews of possible changes for a later release. The previews are available for early evaluation but are not intended to substitute a release.     Importing the SDK Navigate to the QUICKSTART PANEL in the MCUXpresso for VS Code extension. Click on Import Repository. Select the REMOTE option if you have not yet obtained the SDK. Designate a destination to save locally in the Location field.   Select the latest release of the MCUXpresso SDK in the Repository field. The latest version for this walkthrough is MCUXpresso SDK - 24.12.00. Select the main revision in the Revision field.  Note: The SDK can be cloned directly from GitHub. Select the Local option to import if you've already obtained the SDK.   Importing an example project The process of importing a project into MCUXpresso for VS Code does not vary from previous versions. To do so, simply use the Import Example from Repository option.   Exploring the CMake format You will notice several folders when navigating the SDK directory. To examine the CMake project format, let's take a look at the led_blinky_peripheral project. This project is found in examples/demo_apps/led_blinky_peripheral. In this directory, you will find generic project files including the CMakeLists file.   For example, the file that holds the main function in this example project can reference different board files and their respective peripherals.   The files are generic to allow reusability and support for many other devices. This reduces the overall size of the SDK. The CMakeLists file is used to specify the device and project options for the build. In another article, we will cover how the variables in the CMakeLists files are referenced when a build for a specific device is initiated. For now, let's take a look at structure of the file. You'll notice that the variables in this file are generic and will be referenced later for the build. For example, the following two variables are needed for the build system to know which board to build for and where to reference the files. SdkRootDirPath - This specifies the root path to the SDK. board - This specifies the board name.   Once the build is initiated all the necessary files will be drawn in to the project.  
查看全文
Kconfig Usage You can interact with Kconfig via graphical menu interface. Once you have completed the CMake configuration process, you can invoke the Kconfig gui with the following command:   west build -t guiconfig   In this interface, the user selects the options and features desired, and saves a configuration file, which is then used as an input to the build process.   Kconfig Example In this exercise, we will use the simple freertos Hello_World example to demonstrate how to launch and interact with the Kconfig gui. Build the project on the CLI using West       Launch the Kconfig gui by running:        The previous command launches the following gui:       Use the dropdown menus or the Jump to... button to find components   Select a component and click Save to update   Once you have finalized changes to any components, simply rebuild the project.
查看全文
Exploring CLI Build Options In a previous article, we demonstrated how to build a simple project using the CLI. However, we can easily build more complex projects using west build options. We can specify a specific toolchain, compiler, core, etc. To view the complete list of build options run the command: west build -h   Dual Core Device Example For single core devices there is no need to specify a core ID. However, this must be done when working with a dual core device. For example, to build Hello_World for the FRDM MCXN947, the following command needs to be run: west build -b frdmmcxn947 example/demo_apps/hello_world -Dcore_id=cm33_core0   Specifying a Toolchain The MCUXpresso SDK supports several toolchains. To take the example above and build for IAR, we simply specify the IAR toolchain with a build option as follows: west build -b frdmmcxn947 example/demo_apps/hello_world -Dcore_id=cm33_core0 --toolchain iar   Specifying a Different Build Directory As you can see the CLI is quick and easy to use for building projects. So far, we have covered some of the major build options to consider. What happens when we want to evaluate with different builds simultaneously? Well, we can specify different build directories within our workspace. To designate a different build directory for the project above, simply run: west build -b frdmmcxn947 examples/demo_apps/hello_world -Dcore_id=cm33_core0 --toolchain iar -d C:\temp-sdk\mcuxsdk\custom_build *Note the path shown has been personalized. The path for your system will vary.
查看全文
Kconfig Overview Kconfig is a selection-based configuration system originally developed for the Linux kernel. Kconfig is now found more and more in use for other projects beyond the Linux kernel. In the MCUXpresso SDK, Kconfig is used to configure the build in run time which includes component selection with dependency resolve, component configuration with feature enable, disable and customization.   Interface menuconfig and guiconfig are two available interactive configuration interfaces to start a GUI to do run time selection and configuration for Kconfig options. menuconfig is a curses-based interface that runs in the terminal while guiconfig is a graphical configuration interface.   Process Flow The Kconfig files and related prj.conf with priority are put into the Kconfig processor. The direct output is the .config and config headers. Any updates in input Kconfig, output .config and config header will trigger a Kconfig process in next build cmd.   prj.conf is the pre set value for Kconfig symbols. It is the input for the Kconfig process.  The prj.conf search paths can be provided through 3 ways with priority. Fixed prj.conf search paths The priority is from low to high. High priority prj.conf data will override low priority prj.conf data. Specifying customized prj.conf search path in project CMakelists.txt “project” with “CUSTOM_PRJ_CONF_PATH” The “CUSTOM_PRJ_CONF_PATH” argument can be used in project CMakelists.txt “project” macro to specify the customized prj.conf search paths. The prj.conf search paths of CUSTOM_PRJ_CONF_PATH is with higher priority than the fixed prj.conf search paths. -DCONF_FILE=<customized config file> You can directly provide customized prj.conf with -DCONF_FILE=<customized config file>. The customized project config file has the highest priority overall.   Config Headers The Kconfig symbols and the values will be generated into config headers placed in build binary folder. Kconfig symbols and values can also be generated into customized headers. Refer to the online SDK Documentation for this.  
查看全文
Brief Look at MCUXpresso SDK CMake projects   The CMakelists.txt file (as shown above) is used by CMake to configure the project build. This is a text file that contains both standard CMake functions such as include, project, etc. However, for projects found in the MCUXpresso SDK, you will also find MCUXpresso CMake extension functions.  The file shown above displays two MCUXpresso CMake extension functions. mcux_add_source - specifies the path to the project's source files. mcux_convert_binary - specifies the output binary format. For more information regarding this MCUXpresso CMake extension functions, reference the online SDK Documentation.   Building a Project using the CLI Once you have set up your environment and have obtained the MCUXpresso SDK, you can build projects from the command line. To do this, we will be using West commands. To begin, simply launch your preferred CLI and navigate to the directory where you have stored the MCUXpresso SDK. For the complete list of West commands available run: west -h     For this exercise, we will simply build the Hello World example project for the FRDM MCXA153. To do this, the command to run is as follows: west build -b frdmmcxa153 examples/demo_apps/hello_world   Breaking it down The build command that is shown above builds from the root directory of the SDK. In this particular version, the root is the mcuxsdk directory. There are many examples in the MCUXpresso SDK that are supported for many different devices. Hence, there is a need to specify the frdmmcxa153 with the -b flag. Since the build was performed from the root directory, the path to the project was also specified.  
查看全文
MCUXpresso with CMake MCUXpresso aims to greatly reduce build data development and maintenance efforts through the use of CMake. There are many MCUXpresso CMake extensions provided for you to facilitate component, project and misc data record for all toolchains. All extension functions start with prefix mcux_. For the complete list of MCUXpresso CMake extensions, visit the online MCUXpresso documentation. The online documentation explicitly defines all of the MCUXpresso CMake extension functions. This is done through listing argument names, types, and an explanation. Overall, the versatility of managing the build with a custom CMake extension gives the user full control of what goes into their project. In the next section, we will discuss how NXP uses CMake with the SDK examples.
查看全文
Installation The installation process is fairly simple when using the MCUXpresso Installer. The installer automates most of the installation process by installing the following dependencies: Python West CMake Ninja Kconfig Toolchain The MCUXpresso installer can be obtained from MCUXpresso Installer or the MCUXpresso for VS Code extension.  For users that prefer to complete the installation manually, the entire steps can be followed on the MCUXpresso SDK Documentation.   Obtaining the MCUXpresso SDK The SDK is entirely available on GitHub. To obtain the SDK, clone the manifest repository and initialize a west workspace. To do this, open a Command Line Interface(CLI) and run: west init -m https://github.com/nxp-mcuxpresso/mcuxsdk-manifests Once the west workspace has been initialized, update the west projects by running in your designated directory: west update   Exploring The MCUXpresso SDK Once the clone is complete in your designated directory, you will notice two distinct folders besides the .west folder.   The first is the manifests folder. This is the manifest repo which contains the manifest file to initialize and update the west workspace.     The second mcuxsdk folder contains the MCUXpresso SDK source code, examples, middleware integration and script files.     The SDK example projects are found in examples folder within the mcuxsdk folder. Here you will also find all of the other components included in the SDK such as drivers, middleware, and rtos folders.
查看全文
MCUXpresso SDK The MCUXpresso SDK has been reengineered to make use of CMake and Kconfig.   CMake is a software build system that allows easier access and customization of projects obtained from the MCUXpresso SDK. The decision to use CMake was taken with the aim to improve consistency and readability across SDK examples. The MCUXpresso SDK is a comprehensive product including hundreds of boards and devices, thousands of components and examples, for all mainstream toolchains. The MCUXpresso CMake extensions aims to greatly reduce build data development and maintenance efforts. The image below shows the cmakelists.txt file for a sample project in the SDK.   Kconfig is a selection-based configuration system originally developed for the Linux kernel. In MCUXpresso SDK, Kconfig is used to configure the build in run time. This includes component selection with dependency resolve, component configuration with feature enable/disable and customization.    Follow this link for a quick overview exercise that demonstrates how to obtain the SDK and a brief overview on folder structure.
查看全文
Documentation MCUXpresso SDK Documentation  This training currently covers the following areas: MCUXpresso SDK - Intro to CMake and Kconfig  MCUXpresso SDK - CMake and Kconfig: Getting Started MCUXpresso SDK: CMake Usage - Part I   MCUXpresso SDK: CMake Usage - Part II MCUXpresso SDK: CMake Usage - Build Options MCUXpresso SDK: Kconfig Usage MCUXpresso SDK: Kconfig - Exercise MCUXpresso SDK: GitHub + VS Code  MCUXpresso for VS Code: Importing Projects from the MCUXpresso SDK  MCUXpresso for VS Code: Using Kconfig GUI with MCUXpresso SDK Projects     
查看全文
GOAL Learn how to import CMSIS packs into existing projects. In this particular project, CMSIS packs from Crank will be used alongside the freertos_hello example obtained from the MIMXRT1060-EVKB SDK. Note: This walkthrough was adapted from Crank Software's guide included with their CMSIS Pack.   ENVIRONMENT This guide requires MCUXpresso IDE v11.9.1 or latest. MIMXRT1060-EVK SDK version 2.16 or latest.   PROCEDURE 1. Import the freertos_hello example into the workspace. Be sure to set the library type to Newlib (semihost).     2. Rename the project to freertos_sbengine.     3. Add drivers to the project. Right click on the project and select SDK Management -> Manage SDK Components. NOTE: Select Keep Existing and do not replace the FreeRTOSConfig.h file when prompted after adding the following components: Under Drivers -> Device -> SDK Drivers, select: cache elcdif pxp Under Board Components -> Device -> SDK Drivers, select: ft5406_rt Under Software Components -> Device -> SDK Drivers, select: video-common     4. Add additional components to the project. Add the gt911 driver if required by your display. This driver can be found in the MIMXRT1060-EVKB SDK.   Navigate to components/gt911:   Copy the fsl_gt911.c and fsl_gt911.h into the touchpanel directory in the project:     Change the memory manager configuration from the default used by FreeRTOS.   Remove the heap_4.c from the project folder. This is found in freertos/freertos-kernel/portable/MemMang.   Add the heap_3.c into the project folder freertos/FreeRTOS/portable/MemMang. This file can be found in the MIMXRT1060-EVKB SDK.     5. Download the Crank Software pack from Arm Keil | CMSIS Packs.     6. Import the Crank Software pack into MCUXpresso IDE.       7. The Crank Software pack is a graphics bundle that contains six components: Board Display Memory Runtime Libraries Runtime Source Task For this walkthrough, we will add all the components except the Runtime Source component. This component is intended for custom changes. To add the components, right click on the project and select SDK Management -> Add Open-CMSIS Components: Once the components are selected press Ctrl + s to save the components in the project.   8. Resolve conflicts from the previous freertos_hello project configuration. The Board component from the Crank Software pack includes a rewrite of pin_mux.c. Navigate to the board directory of the project and remove the pin_mux.c and pin_mux.h files.   MCUXPresso will automatically add the libraries from the runtime engine into the linker settings. In the project settings remove all the Storyboard engine libraries and plugins. To do this, right click on the project and select Properties. Remove all of the items found under C/C++ Build -> Settings -> Miscellaneous -> Other Objects.   Switch from a managed linker configuration to using the linker file included in the CMSIS pack. In the project settings, navigate to the MCU Linker -> Managed Linker Script. Uncheck the Manage Linker Script option and change the Linker script and Script path. Linker script = MIMXRT1062xxxxx_flexspi_nor.ld Script path= ${cmsis_pack_root}/CrankSoftware/iMXRT10xx/8.1.0/configuration/rt1060/ Note: The path will vary depending on where the user saved the pack.   Copy sbengine_task_pxp_template.c and sbengine_plugins_template.h from the RTE -> Graphics folder into the source folder of the project. Rename these files to remove template  from the name. The project source folder should now look like this:   Exclude the sbengine_task_pxp_template.c and sbengine_plugins_template.h files in the RTE -> Graphics folder from the build.      9. Configure and export a Model C/C++ Header from Storyboard Designer. Create a new project and name it sbengine_model. For this example, I will use a display size of 480x272, color depth RGB 565, and Freetype font manager.   Once the model has been exported, add the header file to the source directory of the project.   Note: For more information about exporting models from Storyboard Designer visit: Crank Storyboard - Exporting and Running on your Embedded Target.     10. Integrating the Storyboard Engine requires modifications to the following: FreeRTOSConfig.h file Locate this file in the source folder of the project and make the following changes: #define configFRTOS_MEMORY_SCHEME 4 #define configUSE_TIME_SLICING 0 #define configENABLE_BACKWARD_COMPATIBILITY 0 #define configTICK_RATE_HZ ((TickType_t)200) #define configUSE_NEWLIB_REENTRANT 0 To this: #define configFRTOS_MEMORY_SCHEME 3 #define configUSE_TIME_SLICING 1 #define configENABLE_BACKWARD_COMPATIBILITY 1 #define configTICK_RATE_HZ ((TickType_t)1000) #define configUSE_NEWLIB_REENTRANT 1   Preprocessor Defines Right click on the project and select Properties -> C/C++ Build -> Settings -> MCU C Compiler. Add the following defines to the “Defined symbols (-D)” pane: SKIP_SYSCLK_INIT XIP_BOOT_HEADER_DCD_ENABLE=1 GRE_TARGET_OS_freertos GRE_TARGET_CPU_cortexm7 GRE_TARGET_TOOLCHAIN_mcuxpresso GRE_FEATURE_VFS_RESOURCES   Change the SDK_DEBUGCONSOLE define from: SDK_DEBUGCONSOLE=0 to SDK_DEBUGCONSOLE=1   If you are using the gt911 touch driver, you will also need to add the following preprocessor define: SDK_I2C_BASED_COMPONENT_USED=1   Library paths. Right click on the project and select Properties -> C/C++ Build -> Settings -> MCU Linker -> Libraries.   In the Library Search path (-L) pane add: "${cmsis_pack_root}/CrankSoftware/iMXRT10xx/8.1.0/storyboard/runtime/freertos-mcuxpresso-cortexm7-swrender-DFP-obj/lib" "${cmsis_pack_root}/CrankSoftware/iMXRT10xx/8.1.0/storyboard/runtime/freertos-mcuxpresso-cortexm7-swrender-DFP-obj/plugins” Note: The path will vary depending on where the user saved the pack. This guide uses the complete configuration of the engine. Therefore, all of the following libraries need to be added in the Libraries pane (-l).  gre greal sbimage sbvfs gre-plugin-animation gre-plugin-lua gre-plugin-poly gre-plugin-circle gre-plugin-timer gre-plugin-logger gre-plugin-screen-path gre-plugin-greio gre-plugin-sbimage-soil gre-plugin-fio_vfs render-plugin-swrender logging-util greio sblua soil swrmgr swrender font-plugin-freetype sbfreetype sbpng sbz   Note: The library order matters. Add the libraries in the order listed above and click Apply and Close     11. Recall that this project was originally the freertos_hello example from the SDK. Therefore, modifications need to be made to the freertos_hello.c file to support the changes for this application. Ensure that the following headers are included: #include "board.h" #include "peripherals.h"   The define for the hello_task_priority is no longer needed and can be removed.    Place the following definitions outside of the main function: void sbengine_main_task(void *argument); void sbengine_input_task(void *argument);   Add the following two additional functions to the initialization sequence in the main() function: BOARD_InitSemcPins() BOARD_InitBootPeripherals().   Replace the hello_task code: if (xTaskCreate(hello_task, "Hello_task", configMINIMAL_STACK_SIZE + 10, NULL, hello_task_PRIORITY, NULL) != pdPASS) with: if (xTaskCreate(sbengine_main_task, "sbengine", 8192, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS)   Add the Storyboard Input handling task creation code block before the call to VTaskStartScheduler: if (xTaskCreate(sbengine_input_task, "StoryboardInput", 2048, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1); }       The source code should now look like this: /* FreeRTOS kernel includes. */   #include "FreeRTOS.h" #include "task.h" #include "queue.h" #include "timers.h"   /* Freescale includes. */ #include "fsl_device_registers.h" #include "fsl_debug_console.h" #include "pin_mux.h" #include "clock_config.h" #include "board.h" #include "peripherals.h"     /******************************************************************************* * Definitions ******************************************************************************/ void sbengine_main_task(void *argument);   void sbengine_input_task(void *argument);   /******************************************************************************* * Code ******************************************************************************/ /*! * @brief Application entry point. */ int main(void) { /* Init board hardware. */ BOARD_ConfigMPU(); BOARD_InitBootPins(); BOARD_InitSemcPins(); BOARD_InitBootPeripherals(); BOARD_InitBootClocks(); BOARD_InitDebugConsole();   if (xTaskCreate(sbengine_main_task, "sbengine", 8192, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; }   if(xTaskCreate(sbengine_input_task, "StoryboardInput", 2048, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while(1); }   vTaskStartScheduler(); for (;;) ; }     NOTE: Check that the line: #include sbengine_model.h in the sbengine_task_pxp.c  file matches the name of the exported header file from Storyboard.   The project should now build:    
查看全文
Documentation eIQ Machine Learning (ML) Software Development Environment Fact Sheet eIQ Toolkit User Guide-This link takes you to the eIQ web page on nxp.com. Once there, click on the Documentation tab or scroll down to the Documentation section   This training currently covers the following areas: Getting Started with eIQ Includes in depth guides on how to get started on i.MX Applications Processors and Microcontrollers FAQs
查看全文
This guide covers: How to import example projects from standalone SDKs How to build, flash and debug How to use the serial monitor
查看全文
The Application Code Hub (ACH) is a repository that contains software examples, code snippets, application software packs and demos developed by NXP experts. ACH provides filter and search options to quickly find specific applications. With the support of Git capabilities, there is an easy way to import and use applications within IDE and tool environments. The Application Code Hub is accessible directly from MCUXpresso for Visual Studio Code and MCUXpresso IDE.    MCUXpresso for Visual Studio Code To access the Application Code Hub, navigate to the QUICKSTART PANEL.     You can use the search bar and the filters to help you find a specific example for your application or hardware.     Once an example is selected the attached README file will open. This file will contain a description of the project as well as technical details.  To import the project, the name field will automatically populate with the example project's name. Designate a location to save the project and click the Import Project(s) button. After, confirm the project and the toolchain at the top of the window as prompted.     If you are prompted to associate a repository, navigate to the PROJECTS section and add the device's SDK to the project. To do this: right click on the project and select Configure > Associate Repository. A dropdown menu will appear on the screen. Select the device's SDK from there. See the Getting Started guide if you have not yet imported the SDK.     You can now build the project. Navigate to the PROJECTS section and click the build button. The project should build successfully.      MCUXpresso IDE To access the Application Code Hub, navigate to the QUICKSTART PANEL.     You'll notice that the UI is slightly different from MCUXpresso for VS Code. However, the search and filtering mechanisms are relatively similar.     To import an example project, simply click on GitHub Link and then the Next button. In the following window click Next to keep the default settings. After, select a destination to store the project and click Next. On the following window, select to import as an existing Eclipse project and click Next. Last verify the project and click Finish.     The project will be added to the Project Explorer view. To build simply select the project in the Project Explorer view and click build.  **Note** The build button can be found in the toolbar at the top, in the Quickstart Panel, or by right-clicking on the project.  
查看全文
FreeMASTER User Guide  This document provides in-depth information about FreeMASTER'S features and usage.    
查看全文