MCUXpresso Training Hub

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Training Hub

讨论

排序依据:
The Application Code Hub (ACH) is a repository that contains software examples, code snippets, application software packs and demos developed by NXP experts. ACH provides filter and search options to quickly find specific applications. With the support of Git capabilities, there is an easy way to import and use applications within IDE and tool environments. The Application Code Hub is accessible directly from MCUXpresso for Visual Studio Code and MCUXpresso IDE.    MCUXpresso for Visual Studio Code To access the Application Code Hub, navigate to the QUICKSTART PANEL.     You can use the search bar and the filters to help you find a specific example for your application or hardware.     Once an example is selected the attached README file will open. This file will contain a description of the project as well as technical details.  To import the project, the name field will automatically populate with the example project's name. Designate a location to save the project and click the Import Project(s) button. After, confirm the project and the toolchain at the top of the window as prompted.     If you are prompted to associate a repository, navigate to the PROJECTS section and add the device's SDK to the project. To do this: right click on the project and select Configure > Associate Repository. A dropdown menu will appear on the screen. Select the device's SDK from there. See the Getting Started guide if you have not yet imported the SDK.     You can now build the project. Navigate to the PROJECTS section and click the build button. The project should build successfully.      MCUXpresso IDE To access the Application Code Hub, navigate to the QUICKSTART PANEL.     You'll notice that the UI is slightly different from MCUXpresso for VS Code. However, the search and filtering mechanisms are relatively similar.     To import an example project, simply click on GitHub Link and then the Next button. In the following window click Next to keep the default settings. After, select a destination to store the project and click Next. On the following window, select to import as an existing Eclipse project and click Next. Last verify the project and click Finish.     The project will be added to the Project Explorer view. To build simply select the project in the Project Explorer view and click build.  **Note** The build button can be found in the toolbar at the top, in the Quickstart Panel, or by right-clicking on the project.  
查看全文
Documentation FreeMASTER Documentation    This training currently covers the following areas: Getting started - Variables, communication with target, and project configuration Gui Guider integration   Other resources NXP Community - FreeMASTER 
查看全文
FreeMASTER User Guide  This document provides in-depth information about FreeMASTER'S features and usage.    
查看全文
Visual Studio Code Documentation  This link leads to the documentation for Visual Studio Code. An overview of VS Code is provided as well as in-depth instructions for all its features.   MCUXpresso for VS Code Wiki  This is a link to the complete MCUXpresso for VS Code documentation. Installation as well as extension settings are covered. An overview of features is also provided.    
查看全文
Open-CMSIS-Pack project  This is a link to the Open-CMSIS-Pack project website. This resource provides all the technical details behind CMSIS-Packs.   Working with Open-CMSIS-Packs  This is a link to documentation for MCUXpresso for VS Code that shows the user how to get started with Open-CMSIS-Packs.      
查看全文
This getting started guide covers: Installation of the MCUXpresso for VS Code extension Dependency installations using the MCUXpresso Installler How to import SDKs
查看全文
This guide covers: How to create a basic gui for your FreeMASTER project using Gui Guider Connection to FreeMASTER How to import FreeMASTER project file How sync the FreeMASTER project variables into a gui
查看全文
This getting started guide covers: Preparation of project variables for visualization with FreeMASTER FreeMASTER communication with target Importing symbol files Adding variables to the FreeMASTER Variable Watch Creating visual components to visualize data for variables
查看全文
This guide covers how to work with example projects obtained from an Open-CMSIS-Pack.
查看全文
This video demonstrates how to quickly get started with Open-CMSIS-Packs  
查看全文