running cst 3.3.2 on ubuntu 23.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

running cst 3.3.2 on ubuntu 23.04

7,957 Views
mastupristi
Senior Contributor I

hello,

I need to run cst 3.3.2 on ubuntu 23.04 to sign using certificates present on an HSM PKCS11 token.

I was able to build cst 3.3.2 using the provided container (based on ubuntu 20.04), and the resulting executable can be launched on ubuntu 23.04

however when it should access the HSM token it would like to load a shared object that does not exist in my FS:

/opt/cst-ssl/lib/engines-1.1/pkcs11.so

 

I have a file of the same name here:

/usr/lib/x86_64-linux-gnu/engines-3/pkcs11.so

which is provided by the libengine-pkcs11-openssl package. I should either force cst to load the library at that location, or copy it to the location where cst looks for it

 

This all seems very tricky to me. What is the correct (or best) way to run cst 3.3.2 on ubuntu 23.04?

 

best regards

Max

0 Kudos
Reply
13 Replies

7,933 Views
marek-trmac
NXP Employee
NXP Employee

Hi Max,

we recommend to run MCUXpresso Secure Provisioning tool on Ubuntu 22.04 LTS 64 bit, with "OpenSSL 1.1.1f 31 Mar 2020" + GNOME recommended (see System requirements).

I'm afraid no one test it on Ubuntu 23.04 yet

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

7,927 Views
mastupristi
Senior Contributor I

Hello Marek,

unfortunately we are forced to use the newer systems like 22.10 and 23.04 because some tools we use are provided and/or can only run on these versions (and later).
In addition we have to use HSM tokens to store private keys, so cst has to be able to access these tokens, consequently I think I have to compile it, or use cst version 3.3.2 which is not integrated with the provisioning tool 6 (which is the latest version available and contains cst 3.2.0)
Finally, the whole thing needs to be run in batch mode within a pipeline of our CI/DC infrastructure, which runs inside a docker container.

best regards

Max

0 Kudos
Reply

7,618 Views
jbhaijy
Contributor III

@mastupristi Can you please share some details how you integrated in CS/CD. We have the same requirement. How you are accessing the HSM through the CST tool? Where HSM is installed, I mean it is connected to build server or some other remote location? 

I have tested signing process with cst-3.3.2 & the softhsm. But we have the API & I don't know how we can call these API with CST tool. 

Please share your experience. Thanks. 

0 Kudos
Reply

7,308 Views
mastupristi
Senior Contributor I

How you are accessing the HSM through the CST tool?

In the .bd file, to be given as input to elftosb (and thus to cst) I specified the "urls" to the HSM token. These urls I derived with the `p11tool` command.

Where HSM is installed, I mean it is connected to build server or some other remote location?

Is connected to the build server

 

I think the problem is related to the version of openssl, its engines, etc....

best regards

Max

0 Kudos
Reply

7,302 Views
jbhaijy
Contributor III

Thanks for reply @mastupristi .

We figured out how CST can help us to sign images with remote HSM with our API's. FYI, CST tool have "Mode = HSM" support that we need to defined in each csf file. Upon execution of cst, it generates the few files which we need to send to signing authority(using API call) to generate the signature. Received signature then insert into CSF binary. 

 

0 Kudos
Reply

7,297 Views
mastupristi
Senior Contributor I

does it works with openssl 3.0.10?

0 Kudos
Reply

7,291 Views
jbhaijy
Contributor III

I tried only with cst-3.3.2. Don't know about earlier version.

0 Kudos
Reply

7,287 Views
mastupristi
Senior Contributor I

maybe we didn't understand each other.

cst 3.3.1 uses (and requires) openssl 1.1.1g
cst 3.3.2 uses (and requires) openssl 1.1.1l

I have ubuntu 23.04 which instead uses (and requires) openssl 3.0.10

so my question (probably rhetorical) is, can one of these versions also work with openssl 3.0.10?

regards

Max

0 Kudos
Reply

7,271 Views
jbhaijy
Contributor III

For cst to work in Mode=HSM, you don't need to build the cst tool along with defined OpenSSL version. I am using Ubuntu-18.04 without building the cst tool. PFA document provided by NXP community member.   

0 Kudos
Reply

7,266 Views
mastupristi
Senior Contributor I

Have you ever tried ubuntu 22.04 or newer?

 

regards

Max

0 Kudos
Reply

7,261 Views
jbhaijy
Contributor III

No

0 Kudos
Reply

7,258 Views
mastupristi
Senior Contributor I

so you can't have any idea whether elftosb and cst can work with openssl >= 3.0, especially for use with USB HSM tokens

regards

Max

0 Kudos
Reply

7,253 Views
jbhaijy
Contributor III

No, I don't have any idea. 

0 Kudos
Reply