blhost on mac failing intermittently?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

blhost on mac failing intermittently?

1,991件の閲覧回数
jackking
Senior Contributor I

I am using a Mac on Mojave 10.14.6, it seems that blhost does not run reliably on Mac...   When running blhost commands from SPT, frequently it will error out. 

I am using the bootloader/flashloader on USB, and tracing the USB bus, I can see that when blhost fails, there is no USB packet sent. 

I try running the blhost command manually from Terminal, and I can see it fail in the same way, only about every 10 executions will blhost send the USB packet, and then get a successful response from the flashloader.

I tried the same from a Windows PC, and blhost runs correctly every single time using the same setup.

I see there is a bug in blhost for Mac that someone identified here: https://community.nxp.com/message/1272499

I tried to make these changes and recompile blhost from the mcu-boot tools included with SDK 2.7, but now get a segfault when using this new compiled version.

0 件の賞賛
返信
0 返答(返信)