SPT GUI not loading after terminal window

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPT GUI not loading after terminal window

ソリューションへジャンプ
5,009件の閲覧回数
nxf64834
NXP Employee
NXP Employee

Hi,

One of our customer has installed SPT v3 on Windows 10, 64 bit, 16GB RAM system . On double clicking the icon on desktop, terminal window comes(refer attached "image") and then disappears. SPT GUI screen is not getting loaded.

How to rectify this issue? 

Please let me know if any other information required.

Thanks!! 

0 件の賞賛
返信
1 解決策
5,001件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi Boby,

see previous post - https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-provisioning-tool-fails-at-startu...- what Region language do you have? Also you can execute it in the command line with "-v" argument, so the prompt window is not closed and error output should not be lost .

liborukropec_0-1626797164105.png

 

Regards,

Libor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,002件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi Boby,

see previous post - https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-provisioning-tool-fails-at-startu...- what Region language do you have? Also you can execute it in the command line with "-v" argument, so the prompt window is not closed and error output should not be lost .

liborukropec_0-1626797164105.png

 

Regards,

Libor

0 件の賞賛
返信
4,979件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Boby,

we have reproduced the issue with unsupported Region settings and the thread was updated with latest info how to workaround the problem. Here is copy of updated info:

> I have reproduced the issue today. It seems SPT does not start if regional format is not listed in https://docs.wxwidgets.org/3.1.4/language_8h.html

> Workaround: select format from the list of supported languages.

> We're sorry for inconvenience.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信