Regarding the issue of mass production of safety tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding the issue of mass production of safety tools

Jump to solution
117 Views
acallamp
Contributor III

HI:

I see that there is an option for UART, but it seems to only support USB?

acallamp_0-1733540370218.png

 

0 Kudos
Reply
1 Solution
91 Views
marek-trmac
NXP Employee
NXP Employee

Hi,

UART should be supported for RT10xx processor, but unfortunately, there is regression problem for RT1xxx processors in manufacturing. We have reproduced the problem on our side, so we will fix this for next release.

As a workaround, can you use MCUXpresso Secure Provisioning tool v9.0.1. There were no significant changes for RT10xx between v9.0.1 and v10, so this should work for you as well.

We're sorry for an inconvenience.

Regards,
Marek

View solution in original post

0 Kudos
Reply
4 Replies
92 Views
marek-trmac
NXP Employee
NXP Employee

Hi,

UART should be supported for RT10xx processor, but unfortunately, there is regression problem for RT1xxx processors in manufacturing. We have reproduced the problem on our side, so we will fix this for next release.

As a workaround, can you use MCUXpresso Secure Provisioning tool v9.0.1. There were no significant changes for RT10xx between v9.0.1 and v10, so this should work for you as well.

We're sorry for an inconvenience.

Regards,
Marek
0 Kudos
Reply
40 Views
acallamp
Contributor III

I installed MCUXpresso Secure Provision tool v9.0.1 and it works fine, but after importing the manufacturing package, burning it with UART failed

 

acallamp_0-1733877191169.png

 

Tags (1)
0 Kudos
Reply
26 Views
marek-trmac
NXP Employee
NXP Employee

Hi,

if you click on the "Failed" label in the 3rd column, it will open the LOG with details about the execution. This should help you understand, what failed.

Regards,
Marek
21 Views
acallamp
Contributor III

HI:

I solved it according to your method. thank you

Tags (1)