MCUXpresso Secure Provisioning v10 BEE USER KEYS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Secure Provisioning v10 BEE USER KEYS

Jump to solution
106 Views
acallamp
Contributor III
HI:
After burning and writing my image through security tools in unsigned, the code can run normally.. No problem...
But when using BEE user keys unsigned encryption, the code does not work properly. Isn't that where the problem lies?. The keys are all the same
 
 
1733448057456.png1733448123207.png1733448222073.png1733448278916.png
0 Kudos
Reply
1 Solution
86 Views
marek-trmac
NXP Employee
NXP Employee

Hi,

I see you have two application "boot" and "app". Which of them does not work? What exactly means "the code does not work properly"?

What exactly mean "The keys are all the same"? I can see you are using single key for BEE Engine 0. Are there any other keys?

Regards,
Marek

View solution in original post

0 Kudos
Reply
2 Replies
87 Views
marek-trmac
NXP Employee
NXP Employee

Hi,

I see you have two application "boot" and "app". Which of them does not work? What exactly means "the code does not work properly"?

What exactly mean "The keys are all the same"? I can see you are using single key for BEE Engine 0. Are there any other keys?

Regards,
Marek
0 Kudos
Reply
81 Views
acallamp
Contributor III
This issue has been resolved because the XIP encryption enable pin in BOOT_CFG [1] was not connected to high
0 Kudos
Reply