Issues using `nxpuuu` to boot an image on i.MX93

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues using `nxpuuu` to boot an image on i.MX93

49 Views
oliben
Contributor II

Hello,

I'm trying to deploy an AHAB image onto my custom board embedding an i.MX93.
I am following this user guide and have reached the  step Image Download step.

Unfortunately, `UUU` appears to be failing:

```

$ nxpuuu -vv -us F06FBE4B3F6142C2 write -f mimx9352 -b emmc ahab_image.bin

spsdk.exceptions.SPSDKError: SPSDK: run_script: returned with exit code -1 and status 0.

```

The same thing happens if I try to run `nxpuuu` with the following script:

```

uuu_version 1.2.39

SDPS: boot -f "ahab_image.bin"

```

If I now try with `uuu` instead, I get a LIBUSB error:

```

3:534-F06FBE 1/ 1 [HID(W): LIBUSB_ERROR_IO (-1) ] SDPS: boot -f "ahab_image.bin"

```

However, the same commands with a different, non-AHAB image, succeed:

```

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.201-0-g727fc2b

Success 0 Failure 0


3:534-F06FBE 1/ 1 [=================100%=================] SDPS: boot -f "imx-boot-imx93.bin-flash_singleboot"

```

Tags (3)
0 Kudos
Reply
0 Replies