DAP to unlock via blhost or SEC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DAP to unlock via blhost or SEC?

ソリューションへジャンプ
1,209件の閲覧回数
NXPMike
Contributor II

lpc55s69

If I set CFPA/CMPA bits to require Debug Authentication Protocol (DAP) for ISP/SWD/JTAG and I want to update my code image via ISP over USB, can I do that using blhost or SEC?

タグ(4)
0 件の賞賛
返信
1 解決策
1,158件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Mike,

I do not know what configuration you have in CFPA/CMPA, so generally:

  • debug authentication can be done only through debug probe
  • ISP communication channels are USB, UART, SPI, I2C
Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,169件の閲覧回数
NXPMike
Contributor II

Thanks for the reply. I was not aware of the nxpdebugmbox utility.

I am still a bit confused. Am I required (in my scenario) to attach a debug probe just to talk to the ISP bootloader via USB once I have enabled ISP DAP? Is there no way to authenticate directly with ISP? SEC/nxpdebugmbox seem to only provide for debug probe connections.

0 件の賞賛
返信
1,159件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Mike,

I do not know what configuration you have in CFPA/CMPA, so generally:

  • debug authentication can be done only through debug probe
  • ISP communication channels are USB, UART, SPI, I2C
Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信
1,194件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello Mike,

a) if you are user of SEC tool, you can use directly SEC GUI to open the debug port - see PKI Management TAB, where you can generate Debug Key, Create a debug request, sign it and then Open the debug port. See User Guide (you can open it from Help menu) and see chapter 7.2 Debug authentication workflow for more details.

b) If you prefer command line, then for opening debug port can be done using nxpdebugmbox utility (also available as an directly executable application in c:\nxp\MCUX_Provi_v10\bin\_internal\tools\spsdk folder (windows, v10)

Please check also Application Note  https://www.nxp.com/docs/en/application-note/AN13037.pdf for more details.

Regards,

Libor

タグ(1)
0 件の賞賛
返信