Application raised an exception error: ValueError

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Application raised an exception error: ValueError

跳至解决方案
1,409 次查看
iann
Contributor III

Hi I'm trying to use V8 of the Secure Provisioning Tool to connect to our MIMXRT1160-EVK and when I select the Debug Probe under the menu Target/Debug Probe it throws an exception straight away without showing the sub menu.   Application raised an exception ValueError.png

Is there a fix for this?

Kind regards

Ian Norman

0 项奖励
回复
1 解答
1,397 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Ian,

Debug Probe menu command is currently not supported for RT116x/7x. The command is supported for processors that contains debug probe selection on toolbar, like for example RW612 (see picture)

marektrmac_0-1716369198975.png

Thank you for reporting the problem, it will be fixed in next release. For now, we recommend to use the button on the toolbar instead of the command. We're sorry for inconvenience.

 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

在原帖中查看解决方案

2 回复数
1,398 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Ian,

Debug Probe menu command is currently not supported for RT116x/7x. The command is supported for processors that contains debug probe selection on toolbar, like for example RW612 (see picture)

marektrmac_0-1716369198975.png

Thank you for reporting the problem, it will be fixed in next release. For now, we recommend to use the button on the toolbar instead of the command. We're sorry for inconvenience.

 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
1,390 次查看
iann
Contributor III
Thanks for the quick response.

Ian
0 项奖励
回复