tftp example to work with lwip

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

tftp example to work with lwip

2,944 次查看
tbiberdorf
Contributor IV

In evaluating the lwip support by the MCUxpresso SDK provided by: Welcome to MCUXpresso | MCUXpresso Config Tools 

As part of the lwip support described, it states that lwip provides support for tftp but there is no demo code provided for tftp and the provided API for tftp will not work until a virtual file system is made available to support it.  I would have guessed that the SDK would have provided an example of how to implement this but they did not.

Can someone provide me a link or documentation on how to build the file system or better an example of how to generate the tftp communication?

thanks

标记 (1)
0 项奖励
回复
1 回复

2,043 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Terry,

I think that the LWIP supports tftp protocol, but we have ported the lwip source code to the UDP and TCP level, and we have developed the file system based on SDHC, but we have not the example code of  tftp example.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复