new flow for CMSIS-DSP use in MCUXpresso SDK 2.12.x?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

new flow for CMSIS-DSP use in MCUXpresso SDK 2.12.x?

2,153 次查看
variable_andrew
Senior Contributor I

The MCUXpresso SDK 2.11.x used to include a .a library file for the CMSIS DSP library.

Now it looks like it provides just source files, (many of which are SUPPOSED to be excluded from the project it seems)?

As there are no DSP demos in the SDK, I was hoping usage would be similar to before, but if I simply create a project using the CMSIS core + DSP source/headers... well it builds there. Then I actually use the DSP functions (including arm_math.h and using functions like arm_mat_init_f32 in c files), I get compiler/linker failures: "multiple definition of `arm_bitreversal_64 ", etc.

 

Anyone else experience this / have a solution?

Screen Shot 2022-11-15 at 10.44.53 AM.png

标记 (2)
0 项奖励
回复
4 回复数

1,228 次查看
isaac2022
Contributor I

If you include the sources for CMSIS DSP, mcuxpresso will compile and link the code into your executable.   You should then remove the library from your project settings.  The static, precompiled libraries are no longer being provided as part of CMSIS DSP distribution,

0 项奖励
回复

2,147 次查看
variable_andrew
Senior Contributor I

i reverted JUST the CMSIS DSP library (as per the screen shot below, so back to 5.0.3 it seems), which means bringing back the .a binary lib file, updating the project to look for that lib file in the linker/asm project settings, and the project builds w/ the new 2.12.x SDK (but old CMSIS DSP) just fine, so it seems to me something may be broken in the new CMSIS DSP?

Screen Shot 2022-11-15 at 3.45.27 PM.png

0 项奖励
回复

2,138 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @variable_andrew ,

Can you share your project?

 

Regards,

Jing

0 项奖励
回复

2,077 次查看
variable_andrew
Senior Contributor I

Coming back to this - to reproduce basic build problems w/ this SDK and ARM CMSIS DSP functions, start with a fresh project:

Screen Shot 2023-01-27 at 9.22.35 AM.pngScreen Shot 2023-01-27 at 9.22.46 AM.png

add in the CMSIS DSP library header... then verify what CMSIS components are included...

 

Screen Shot 2023-01-27 at 9.23.16 AM.png

I linked the application to RAM to avoid messing w/ any FLASH setup, etc etc, then FINISH creating the project:Screen Shot 2023-01-27 at 9.25.08 AM.png

 

Add the following to the main project to test the DSP availability (and call this function from main):

/* TODO: insert other include files here. */
#include "arm_math.h"

/* TODO: insert other definitions and declarations here. */
static void test_matrix_transpose();

static void test_matrix_transpose(){
  arm_matrix_instance_f32 A;      /* Matrix A Instance */
  arm_matrix_instance_f32 AT;     /* Matrix AT instance */
  arm_status status;

  float32_t A_f32[8*3] = {0};
  float32_t AT_f32[3*8];

  for (int i=0; i< 8; i++){
    A_f32[i * 3 + 0] = 1;
    A_f32[i * 3 + 1] = 2;
    A_f32[i * 3 + 2] = 3;
  }

  /* Initialize A Matrix Instance with numRows, numCols and data array */
  arm_mat_init_f32(&A, 8 /*rows*/, 3 /*cols*/, (float32_t *)A_f32);
  /* Initialize Matrix Instance AT with numRows, numCols and data */
  arm_mat_init_f32(&AT, 3, 8, AT_f32);
  /* calculation of A transpose */
  status = arm_mat_trans_f32(&A, &AT);

  if (status != ARM_MATH_SUCCESS) {
    while (1);
  }
}

 

Then, try and build - see errors:

build fails despite includint arm_math.h which includes the specified matrix functionsbuild fails despite includint arm_math.h which includes the specified matrix functions

 

 

If i just include the library headers in the project and not the source, before this would include the actual .a file (the compiled library itself), but if you go to project settings, linker, library: the library is no where to be found.

 

no library anymoreno library anymore

0 项奖励
回复