is it possible that different version of MXUXpresso use different versions of SDK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

is it possible that different version of MXUXpresso use different versions of SDK?

跳至解决方案
2,052 次查看
ping1
Contributor V

Dear all

I am trying new SDK with new IDE , both v24.12.0, use RT1024-EVK, however, when i install new SDK, it overwrite the old v2.12.0, which is my current projects based on and works with v11.8 IDE, I wonder whether it is possible that my new IDE use a different SDK location, that is not interfere with existing SDK? I will update it when I am totally happy with new one.

Thanks in advance.

Ping

 

标记 (3)
0 项奖励
回复
1 解答
1,703 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ping1 

I am apologize for the delayed response. 

I am sharing your feedback internally, so the team is aware of your issues and needs, sorry for the trouble.

Yes, we want users to update always to the latets versions of the IDE,  we are always providing new releases with improments, new features, new supported mcus and bug fixes.

 

Diego

在原帖中查看解决方案

0 项奖励
回复
7 回复数
2,046 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ping1 

Thank you for contacting us.

Would be possible for you to try the Enable SDK/manifest versions swith option. You should  be able to install different versions of an SDK, when  this option is enabled.

If you are getting troubles to get the two versions , please report them to me,  along your OS. Please to reestart the MCUXpresso IDE, after enabling this option, a computer restart will do the job.

This option is under Preferences, please take a look at the below figure. 

Snag_6d1fff4b.png

Best regards,

Diego

 

2,032 次查看
ping1
Contributor V

Thank you for Reply, Diego

I have added my User defined folder, however, I could not remove the the Common folder SDK, I am intended to let one IDE use User defined folder, and another version use Common folder, however the User Defined one sees both. is that intended?

It is not a big issue now, although.

Regards!

Ping

0 项奖励
回复
2,028 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ping1 

Thank you for your reply!

Ok, I understand that you selected different SDK locations for two different IDE versions. 

 

Snag_71d47a95.png

Could you detail more about this User Defined one sees both?  If  set my MCUXpresso IDE v24.12 [Build 148] [2025-01-10]  to User defined,  I will see that the SDKS from the common folder and my user defined folder are still available in the Installed SDKs window? Could you provide  a picture?

Diego

 

 

0 项奖励
回复
2,004 次查看
ping1
Contributor V

Thanks for reply

 

Here is the picture, it shows User Defined one - under o4 folder, which I created, also shows common one in folder ..02\SDKPackage although I didn't choose it.

In installed SDL Tab under IDE, it shows both too, I am using new IDEv24.12, BTW.

Regards!

Ping

 
 

 

0 项奖励
回复
1,995 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ping1 

Thank you for your kind response.


So, let us say that basically the problem is that you need new IDEv24.12, to not erase your older SDK versions when installing latest versions ( let me know otherwise). I still need to determine if this a bug and see if I can recommend another solution. I do appreciate your help so far, even though it is not a critical topic for you!


So, if you remove the 02/SDK/Packages ( common folder) and restart the new IDEv24.12 and then restart the IDE, you see that the IDE will still fetch the common folder, I am correct?

Snag_780c2c86.png

Thank you! 

Diego

 

 

0 项奖励
回复
1,966 次查看
ping1
Contributor V

Hi, Diego

You are right, I would like to use two different versions of IDE with separate SDKs totally.

I removed SDKS in the common folder, and then it doesn't appear on IDE24.12, but it also doesn't appears on my v11.8 IDE which is all existing project based on .

Or shall i not upgrade the IDE at all? not long ago, I thought v11.8 is your final IDE version and you are moving to something else, but now another new version with big jump, as I am starting a new project, I think it is better to start with new IDE and latest SDKs.

Regards!

Ping

0 项奖励
回复
1,704 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ping1 

I am apologize for the delayed response. 

I am sharing your feedback internally, so the team is aware of your issues and needs, sorry for the trouble.

Yes, we want users to update always to the latets versions of the IDE,  we are always providing new releases with improments, new features, new supported mcus and bug fixes.

 

Diego

0 项奖励
回复