how to use lwip_mpc5748g

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use lwip_mpc5748g

2,567件の閲覧回数
gangzhou
Contributor II

Hi,

I am using s32 design studio for NXP #mpc5748g enet dev kit. Here LWIP example code "lwip_mpc5748g" integrated with freertos by default.But ,when  ping the ip address of MPC5748G dev kit,it dose not reply.I want to know how to use this example.How to config the board as client or server?

タグ(2)
0 件の賞賛
返信
5 返答(返信)

2,373件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

root cause of this issue is that LwIP example cannot handle ARP protocol, so you must add MAC address of the board manually into PC ARP cache.

Run command line as an administrator and use the command shown in the figure below.

pastedImage_1.png

Addresses used in the figure are the default ones in the lwip project.

Regards,

Martin

0 件の賞賛
返信

1,187件の閲覧回数
H-chips
Contributor III
Hello, may I ask why I can't ping the MAC address after manually adding it to the arp cache of the pc。
0 件の賞賛
返信

2,373件の閲覧回数
gangzhou
Contributor II

thank you for your reply.if I want to use the devkit board as  server with example code "lwip_mpc5748g" what,should I do? 

0 件の賞賛
返信

2,373件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

it depends on what server do you mean. Here are possibilities, which LwIP provides

Operating systems that implement the lwIP TCP/IP stack may provide a range of supporting clients and servers at the application layer. Such as an IPv4 DHCP (Dynamic Host Configuration Protocol) client or IPv4 Link-local addresses (aka. AutoIP). Specialized raw API applications include: an HTTP server, a SNTP client, a SMTP client, a NetBIOS nameserver, a mDNS responder, a MQTT client and a TFTP server.

But all of this implementation must be done on your own. There is no example available.

Regards,

Martin

0 件の賞賛
返信

2,373件の閲覧回数
gangzhou
Contributor II

Tkank you!

0 件の賞賛
返信