flexio camera

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

flexio camera

跳至解决方案
918 次查看
seobi
Contributor III

Hi, We are planning to use a parallel camera with FlexIO on the EVKBRT1170.

Referring to the RT1010 sample, we have two questions during the implementation:

1. The PCLK on the RT1010 is said to support up to 20MHz. How much is supported in the case of the RT1170? I couldn't find this information in the datasheet.

2. The sample for the RT1010 is for 8-bit data, but in our case, we need to use 16-bit data. Is it possible to obtain a sample for this? If not, could you guide us on what needs to be modified?

Best regards,

0 项奖励
回复
1 解答
846 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seobi,

1. The PCLK frequency can be as high as the Clock Source frequency that the FlexIO admits. For the case of the RT1170, this would equate to a maximum of 120MHz.

2. I'm afraid that only 8-bit data is supported for the parallel camera emulated with FlexIO. I apologize for the inconvenience this may cause.

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
1 回复
847 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seobi,

1. The PCLK frequency can be as high as the Clock Source frequency that the FlexIO admits. For the case of the RT1170, this would equate to a maximum of 120MHz.

2. I'm afraid that only 8-bit data is supported for the parallel camera emulated with FlexIO. I apologize for the inconvenience this may cause.

BR,
Edwin.

0 项奖励
回复