Why was WiFi QCA removed from SDK 2.9.0 for LPC55s69?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why was WiFi QCA removed from SDK 2.9.0 for LPC55s69?

Jump to solution
1,591 Views
danielkrol
Contributor III

Hello,


Why was WiFi qca demo (WiFi 10 Click module) and middleware library removed from SDK 2.9.0 for LPC55s69?

Regards,
Daniel

0 Kudos
1 Solution
1,531 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, the new solution will use also MicroBUS. It will use UART for communication using AT commands.

View solution in original post

0 Kudos
6 Replies
1,576 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Yes, we have removed support for this old Qualcomm platform, we are planning to focus for mw320 based UART connected WiFi.

Marvel Wifi will be the main choices for NXP SDK.

 

Have a nice day,

Jun Zhang

 

Best Regards

Jun Zhang

0 Kudos
1,549 Views
danielkrol
Contributor III

Hi, 

Thank you for the information.

It's a pity because the Wifi 10 Click module (SX-ULPAN-SB-2401) is relatively short on the market. We use it at the University in our Embedded and IoT laboratory with LPC55s69 EVB (we have 20 teaching positions ). It remains for us to port the library from the older SDK. 

BTW we also have LPC54018 IoT modules (also QCA WiFi).

In the case of the aforementioned MW320, do you plan to release any module with a Micro BUS or PMOD connector, easy to connect to existing evaluation boards such as LPC55s69 EVB?

 

Regards,

Daniel

0 Kudos
1,532 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, the new solution will use also MicroBUS. It will use UART for communication using AT commands.

0 Kudos
1,526 Views
danielkrol
Contributor III

Hi,

Thanks for the information.

So we are waiting impatiently. When can this be expected?

Regards,
Daniel

0 Kudos
1,520 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

 We will be releasing the support during Q2 2021

0 Kudos
1,517 Views
danielkrol
Contributor III

Thanks.

Regards,
Daniel

0 Kudos