Why is the sdmmc/port folder and files not configured for a new project?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why is the sdmmc/port folder and files not configured for a new project?

跳至解决方案
1,914 次查看
minibix
Contributor II

Hi,

In example projects the sdmmc/port folder is present with the correct port source files based on the mechanism used respond to changes in the sdmmc stack (i.e. interrupt, polling or FreeRTOS).

When you create a new project, the port folder is not copied in... just 'inc' and 'src' are copied in.

Is there a reason for this? Or is there another configuration step to have this configured automatically?

At the moment I am creating a new project and copy/pasting from the SDK zip file.

(I am using MCUX 10.2 and SDK 2.3.1 for MK22FN1M0xxxx)

标记 (3)
0 项奖励
回复
1 解答
1,711 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Mike

Thanks for your feedback, it seems an issue in this release.

The source in port folder is a wrapper to compatible with different hosts. For temp solution, you can add this folder manually.

This issue will be fixed in future release.

Regards

Daniel

在原帖中查看解决方案

2 回复数
1,712 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Mike

Thanks for your feedback, it seems an issue in this release.

The source in port folder is a wrapper to compatible with different hosts. For temp solution, you can add this folder manually.

This issue will be fixed in future release.

Regards

Daniel

1,711 次查看
minibix
Contributor II

Great, thanks.

To note, this issue was also in MCUX 10.1 and SDK v2.3.0.

0 项奖励
回复