Hi Manuel Malagon,
Do you try to add the breakpoint, whether it works and stop or not?
Do you try any other SDK simple project, eg, helloworld, ledblinky, whether the single step works or not?
You can also add some screen shoots to demonstrate your issues.
Could you please try the breakpoint instead of the F6 F5, and check another SDK project, just check it is related to the project or the IDE.
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------