Where is the SE050 SDK Package for i.MX RT 1050?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the SE050 SDK Package for i.MX RT 1050?

960 Views
TomGibson
Contributor III

In this video on the NXP YouTube channel I can see a package to use the SE050 with i.MX RT 1050 is provided: https://www.youtube.com/watch?v=tKqbC-ipcr

However on the EdgeLock SE050 page there is only an SDK Package for i.MX RT 1060. Where is the package for i.MX RT 1050? Furthermore the MCUXpresso SDK for i.MX RT 1060 from the SDK builder includes the se_hostlib packages and a few samples (such as se05x_minimal) , whereas the i.MX RT 1050 SDK does not. Why is this? Where can we get the relevant SE050 SDK files for i.MX RT 1050?

The only major functional difference between these two MCUs is the additional 512k OCRAM on the 1060 which the 1050 does not have, this does not explain why the SDK package only appears to be published for one of the two.

0 Kudos
1 Reply

945 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @TomGibson ,

 

Actually there was some earlier version supporting i.MX RT 1050 , but now it is discontinued and supports 1060 instead. so it is still possible to use the packet for 1050 but with old MW, alternatively you have to port the latest 1060 package to 1050, please kindly refer to the porting guide as below for details.

https://www.nxp.com/docs/en/application-note/AN12448.pdf

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------