Where can I get KSDK for MCU MK61FX512?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I get KSDK for MCU MK61FX512?

1,205 Views
tenishevram
Contributor I

MCUXpresso SDK Builder does not support my MCU. But I need SDK for my MCU where can I get it?

0 Kudos
5 Replies

1,109 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Ramil:

MK61 belongs to K70 series and NXP does not support it in SDK. Currently no plan to support it in SDK.

One solution is to use MQX 4.2. which has MFS driver that includes support to Nand Flash and DDR memories.

So we can create a new BSP for MK61 based on TWR-K70F120M, which has a MCU quite similar to K61,

you also can use bare metal project.

Regards

Daniel

0 Kudos

1,049 Views
omkardixit
Contributor III

I'm also having the same issue. I was searching SDK for the TWR-K70F120M almost everywhere. Now when I read you are not planning to support K70 SDK I'm really disappointed. I don't know how I can work now!

0 Kudos

1,109 Views
tenishevram
Contributor I

Hi Daniel,

Maybe do you have old versions of SDK for MK61?

0 Kudos

1,109 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Ramil:

For bare metal code, please download it from below link

TWR-K70F120M|Tower System Board|Kinetis MCUs | NXP 

pastedImage_3.png

For MQX, you can download it from below link. K70 is very similar to K61.

MQX™ Software Solutions - Releases and Patches | NXP 

Regards

Daniel

0 Kudos

1,109 Views
tenishevram
Contributor I

Yes It would be great if you provide me BSP for MK61 which I can use in bare metal projects.

Regards

Ramil

0 Kudos