I'm using the FRDM-K66F board and running the freertos_uart demo project. It works well enough through UART0, but this is carried through the USB debug connection and I need to look at the signal on the wire. I changed the demo project to use UART1 instead by the following steps:
1. Connect pins A9 and A11 to UART1 TX and RX by updating pin_mux.c
2. Change the DEMO_UART* symbols to refer to UART1 instead of UART0
3. Connect J1 pin 4 to pin 2 on the DE9 serial connector.
4. Connect J1 pin 2 to pin 3 on the serial connector.
5. Connect J3 pin 12 to pin 5 on the serial connector.
I can see that pin 2 on the serial connector is where I want to transmit because my script that watches the port picks up the noise when I disconnect and reconnect that wire. I've stepped through the code and see that the UART_WriteNonBlocking function is entered and eight characters are written to the D register on each pass until the last one which only has seven. So it seems we've done the right thing, but nothing is seen on the other end. I can see also that the UART1 driver IRQ handler is invoked.. This really looks like a pin issue. When I get to the receive part of the demo, the software always ends up terminating on a timeout on the event group wait.
Any experience with this out there?
解決済! 解決策の投稿を見る。
Hi Jeremy Anderson:
I did a quick test according to your modifications. I tested with my uart-to-usb , and it can work on my side.
My modifications :
1. pin_mux.c
void BOARD_InitPins(void) {
CLOCK_EnableClock(kCLOCK_PortC); /* Port B Clock Gate Control: Clock enabled */
PORT_SetPinMux(PORTC, PIN3_IDX, kPORT_MuxAlt3); /* PORTB16 (pin E10) is configured as UART0_RX */
PORT_SetPinMux(PORTC, PIN4_IDX, kPORT_MuxAlt3); /* PORTB17 (pin E9) is configured as UART0_TX */
}
2 freertos_uart.c
#define DEMO_UART UART1
#define DEMO_UART_CLKSRC SYS_CLK
#define DEMO_UART_CLK_FREQ CLOCK_GetFreq(SYS_CLK)
#define DEMO_UART_RX_TX_IRQn UART1_RX_TX_IRQn
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hOne more note on this. I found that the data I was getting on the console side was inverted when using UART1. I set the TXINV bit in register C3 and everything looks good from the transmit standpoint. I still don't get anything back on the receive pin (J1-2). Why would UART1 present mark for space with respect to UART0?
OK, thanks Daniel. I see what is going on now. The TTL levels at the pins present inverted values when connected to the RS-232 lines on my docking station serial port. This turns out to have been a matter of my own ignorance, now remedied. Thanks for the help!
Hi Jeremy Anderson:
I did a quick test according to your modifications. I tested with my uart-to-usb , and it can work on my side.
My modifications :
1. pin_mux.c
void BOARD_InitPins(void) {
CLOCK_EnableClock(kCLOCK_PortC); /* Port B Clock Gate Control: Clock enabled */
PORT_SetPinMux(PORTC, PIN3_IDX, kPORT_MuxAlt3); /* PORTB16 (pin E10) is configured as UART0_RX */
PORT_SetPinMux(PORTC, PIN4_IDX, kPORT_MuxAlt3); /* PORTB17 (pin E9) is configured as UART0_TX */
}
2 freertos_uart.c
#define DEMO_UART UART1
#define DEMO_UART_CLKSRC SYS_CLK
#define DEMO_UART_CLK_FREQ CLOCK_GetFreq(SYS_CLK)
#define DEMO_UART_RX_TX_IRQn UART1_RX_TX_IRQn
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Just one more note here, I see in your example the comments indicate UART0 (cut and pasted I'm sure) but these actually connect PORTC3 (pin A11) and PORTC4 (pin A9) to UART1.
OK, partial answer. My eyes are going, but sending the same message over the UART0 link results in a coherent transmission, whereas UART1 ends up sending an extra byte and none of it makes any sense. It looks like noise might be an issue since this is a kludged up experiment.