Hello ,
I am working on the LPC546xx based device.
I intend to use the timer for generating interrupt at various time interval.
I came across various timers
1. Multi-Rate Timer (MRT)
2. Repetitive Interrupt Timer (RIT)
3. System tick timer (SYSTICK)
4. Micro-tick Timer (UTICK)
5. CTimer
6. SCTimer/PWM
Is there any document/application note given info of comparison of timer, when to use, interrupt priority, interrupt latency..
regards,
Hemanth
解決済! 解決策の投稿を見る。
Hi, Hemanth,
First of all, let's talk about the interrupt priority, interrupt latency, the interrupt priority and interrupt latency are core attributes, the LPC546xx uses Cortex-M4, it supports the nested interrupt mechanism(preemptive interrupt mechanism), each interrupt can be set up with an individual priority level. Each interrupt has the the same interrupt latency, it is not related to interrupt priority.
Regarding the function of different Timer modules, I do not think there is application note which focuses on the comparison. But I can give a review.
1)SCTimer/PWM: can generate complicated PWM signal to control even motor, have capture function, can generate interrupt with programmable interval, can be a frequency divider.
2)CTimer: can generate simple PWM signal, can generate interrupt with programmable interval, has capture function, can be a frequency divider.
3)Multi-Rate Timer (MRT): can only generate interrupt
4)Repetitive Interrupt Timer (RIT): can only generate interrupt
5)System tick timer (SYSTICK): can generate interrupt for core
6)Micro-tick Timer (UTICK): can generate interrupt, and have capture function
Hope it can help you
BR
Xiangjun Rong
Hi, Hemanth,
First of all, let's talk about the interrupt priority, interrupt latency, the interrupt priority and interrupt latency are core attributes, the LPC546xx uses Cortex-M4, it supports the nested interrupt mechanism(preemptive interrupt mechanism), each interrupt can be set up with an individual priority level. Each interrupt has the the same interrupt latency, it is not related to interrupt priority.
Regarding the function of different Timer modules, I do not think there is application note which focuses on the comparison. But I can give a review.
1)SCTimer/PWM: can generate complicated PWM signal to control even motor, have capture function, can generate interrupt with programmable interval, can be a frequency divider.
2)CTimer: can generate simple PWM signal, can generate interrupt with programmable interval, has capture function, can be a frequency divider.
3)Multi-Rate Timer (MRT): can only generate interrupt
4)Repetitive Interrupt Timer (RIT): can only generate interrupt
5)System tick timer (SYSTICK): can generate interrupt for core
6)Micro-tick Timer (UTICK): can generate interrupt, and have capture function
Hope it can help you
BR
Xiangjun Rong