The following items are not supported or not valid SDKs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The following items are not supported or not valid SDKs

2,968件の閲覧回数
eljeffo
Contributor III

After building my SDK using:

MCUXpresso SDK|NXP 

Then dragging and dropping said zip file into MCUXpresso I get the following message:

"The following items are not supported or not valid SDKs"

I verified the zip file was built for all platforms.

Is there anything else that I should have done?

タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,663件の閲覧回数
eljeffo
Contributor III

Hi Lukas,

Here's you can find the result of my request and manifest.xml at the following link:

https://www.evernote.com/l/AE-MLk0ko0lHIb4CELjZZlA9CcjqutEZ8s8 

I've included both the importable and non-importable versions for your reference.

0 件の賞賛
返信

2,663件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Jeff,

Thanks for sharing. Is it possible that you switched two packages by mistake? The FRDM-KE15Z_manifest.xml file you shared is not related to MKV31F512xxx12/FRDM-KV31F device/board, instead it contains data for MKE15Z256xxx7/FRDM_KE15Z.

Also please note that in case of existing SDK packages generated on MCUXpresso SDK web prior to March 22nd, these packages does not  support MCUXpresso IDE and has to be regenerated to be able to use them in the MCUXpresso IDE.

Regards,

Lukas

0 件の賞賛
返信

2,663件の閲覧回数
enore_grattoni
Contributor I

I see that USB stack is not selected on download

Immagine.jpg

this is config

pastedImage_2.png

now I will try to reset config and download again

0 件の賞賛
返信

2,663件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hello Jeff,

can you share the *_manifest.xml file from the root directory of the SDK package that failed to import into MCUXpresso IDE?

Thank you,

Lukas 

0 件の賞賛
返信

2,663件の閲覧回数
eljeffo
Contributor III

Aha... the IDE is confused unless MCUXpresso is the only platform in the zip file.

0 件の賞賛
返信