MCUXpresso SDK (2.6.2) seems to be missing time support, at least as far as the C standard library (C90, C99) is concerned. I need to convert snvs_hp_rtc_datetime_t to time_t, which is what mktime() would normally do, but that requires a struct tm. Alternatively, if time were available as, or convertible to, type time_t, I could work with that.
I'm using the MIMXRT1062DVJ6A with MCUXpresso 2.6.2. I also need millisecond time resolution, but the SNVS doesn't seem to provide that.
Hi Jeff Thompson
Yes, as we are working in a embedded system, we tried to optimize our resources, this is why the datetime structure is like:
// typedef struct _snvs_hp_rtc_datetime
// {
// uint16_t year; /*!< Range from 1970 to 2099.*/
// uint8_t month; /*!< Range from 1 to 12.*/
// uint8_t day; /*!< Range from 1 to 31 (depending on month).*/
// uint8_t hour; /*!< Range from 0 to 23.*/
// uint8_t minute; /*!< Range from 0 to 59.*/
// uint8_t second; /*!< Range from 0 to 59.*/
// } snvs_hp_rtc_datetime_t;If you need it, you could create a new time variable with the structure of time.h :
// struct tm
// {
// int tm_sec; /* seconds after the minute, 0 to 60
// (0 - 60 allows for the occasional leap second) */
// int tm_min; /* minutes after the hour, 0 to 59 */
// int tm_hour; /* hours since midnight, 0 to 23 */
// int tm_mday; /* day of the month, 1 to 31 */
// int tm_mon; /* months since January, 0 to 11 */
// int tm_year; /* years since 1900 */
// int tm_wday; /* days since Sunday, 0 to 6 */
// int tm_yday; /* days since January 1, 0 to 365 */
// int tm_isdst; /* Daylight Savings Time flag */
// };
Sorry for the inconvenieces that this may cause you.
Best regards
To assist you properly,can you please provide us the part number that you are using?