SDK v2.15.0 for RT1050 - Defining I2C_RETRY_TIMES causes compile error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK v2.15.0 for RT1050 - Defining I2C_RETRY_TIMES causes compile error

ソリューションへジャンプ
4,277件の閲覧回数
dmarks_ls
Senior Contributor II

There are fatal code problems in fsl_flexio_i2c_master.c (FSL_FLEXIO_I2C_MASTER_DRIVER_VERSION is 2.5.0).  If I set I2C_RETRY_TIMES in my preprocessor defines to a non-zero value, I get multiple compiler errors, all declaring that "waitTimes" is undefined.  There is also a warning about a declaration of "waitTimes" being unused.  It appears that this build configuration was never tested prior to release.

The solution/workaround is to declare waitTimes in appropriate locations and to remove the unused location.  I have attached a fixed version of the C file; please review and merge into your next release, thanks.

Dana M.

0 件の賞賛
返信
1 解決策
4,251件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @dmarks_ls 

I reproduce this issue, thanks for your information.

And I will report this issue to our SDK team.

Best regards,
Hang

 

元の投稿で解決策を見る

2 返答(返信)
3,996件の閲覧回数
sachin_patel
Contributor IV

Hi,

I reported this issue to NXP in March 2023 as can be seen here: Compile-Error-in-MCUXpresso-SDK-v2-13-0-v2-14-0-and-v2-15-0-fsl/m-p/1698607.

As of SDK v2.16 on my device which released earlier today, this issue still has not been resolved. Can you check if it has been resolved on your device?

Thanks,

Sachin Patel

4,252件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @dmarks_ls 

I reproduce this issue, thanks for your information.

And I will report this issue to our SDK team.

Best regards,
Hang