There are fatal code problems in fsl_flexio_i2c_master.c (FSL_FLEXIO_I2C_MASTER_DRIVER_VERSION is 2.5.0). If I set I2C_RETRY_TIMES in my preprocessor defines to a non-zero value, I get multiple compiler errors, all declaring that "waitTimes" is undefined. There is also a warning about a declaration of "waitTimes" being unused. It appears that this build configuration was never tested prior to release.
The solution/workaround is to declare waitTimes in appropriate locations and to remove the unused location. I have attached a fixed version of the C file; please review and merge into your next release, thanks.
Dana M.