(SDK) usb MIDI device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

(SDK) usb MIDI device?

Jump to solution
4,752 Views
mmlee
Contributor II

Hello,

Is there any chance we will get a midi device class implementation for the USB middleware?

Is it something that's in the pipeline?

1 Solution
4,516 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I am afriad of the imxrt family there is not the SDK for it.

View solution in original post

5 Replies
4,390 Views
BetoGreen
Contributor III

Looks like the example is not complete....


audio_generator.c is missing, the webpage shows usb_device_descriptor.c twice.

Does anyone have the real audio_generator.c file they can post here?

0 Kudos
Reply
4,514 Views
ogawatakeshi
Contributor II

Hello

A simple example is implemented using MCUXpresso USB Stack.
Referenced projects(dev_audio_generator_bm)

modify following code

pastedImage_1.png

Please refer to the following article

MCUXpressoSDK USB StackでMIDIStreamingSubClassを使う2 - がれすたさんのDIY日記 

(Sorry in japanese......

0 Kudos
Reply
4,514 Views
Pavel
NXP Employee
NXP Employee

NXP LSDK supports USB MIDI driver. For example see the following documents:

https://www.nxp.com/docs/en/user-guide/LS1028ABSPUG.pdf

 

https://www.nxp.com/files-static/soft_dev_tools/doc/support_info/QorIQ-LS1012A-SDK-v0.4.pdf?&fasp=1&...

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,514 Views
mmlee
Contributor II

Any chance we get it to the IMXRTxx series as well? 

0 Kudos
Reply
4,517 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I am afriad of the imxrt family there is not the SDK for it.