SDK for deprecated EVK-MIMXRT1050

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK for deprecated EVK-MIMXRT1050

1,222件の閲覧回数
mikebez
Contributor I

Hi.

On https://mcuxpresso.nxp.com/en/select  there are two boards for RT1050:

EVK-MIMXRT1050, with "KSDK 2.3.0  (released 2018-01-11)"

EVKB-IMXRT1050, with "KSDK 2.4.0  (released 2018-05-25)"

Will EVK-A be updated to 2.4.0?

タグ(2)
0 件の賞賛
返信
1 返信

990件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Mike,

Yes, the KSDK 2.4.0 can work on KSDK 2.4.0 board. Both this two version BSP can work on EVK-A. But EVKB-IMXRT1050 only support KSDK 2.4.0.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信