SDK for deprecated EVK-MIMXRT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK for deprecated EVK-MIMXRT1050

853 Views
mikebez
Contributor I

Hi.

On https://mcuxpresso.nxp.com/en/select  there are two boards for RT1050:

EVK-MIMXRT1050, with "KSDK 2.3.0  (released 2018-01-11)"

EVKB-IMXRT1050, with "KSDK 2.4.0  (released 2018-05-25)"

Will EVK-A be updated to 2.4.0?

0 Kudos
Reply
1 Reply

621 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Mike,

Yes, the KSDK 2.4.0 can work on KSDK 2.4.0 board. Both this two version BSP can work on EVK-A. But EVKB-IMXRT1050 only support KSDK 2.4.0.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply