Hi all,
regarding SDK 2.6.0 for LPC54616J512 I have detected an issue when configuring a New project from Wizard. Under Operating Systems and Middleware Tabs I can select anything (Freertos and USB Stack) because they are disabled. However, LPC54618J512 works fine. I think there is a problem related to manifests.xml because I am not able to configure these options when both MCUs have same peripherals functionalities.
Regards
Hello Javier S ,
I have report this issue to related team.
Now the workaround is: Create a new project based on LPC54618J512, add the Middleware you need,
then copy the generated files into LPC54616j512 project, they are the same in both chips.
Hope it helps,
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------