RT1176 debug console and shell

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1176 debug console and shell

1,205件の閲覧回数
DanielTC
Contributor I

Under SBR\SDK_2_15_100_MIMXRT1170-EVK\devices\MIMXRT1176\utilities

How do you build the debug console and shell?

Or can you add the utilities directory to an existing project?

0 件の賞賛
返信
3 返答(返信)

1,178件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @DanielTC,

You can add these utility components when creating a new project on the components section:

EdwinHz_0-1718297927173.png

Or for an existing project, you can open the SDK component manager window and select them there:

EdwinHz_1-1718297966297.png

EdwinHz_2-1718297973035.png

BR,
Edwin.

 

0 件の賞賛
返信

1,148件の閲覧回数
DanielTC
Contributor I

I'm using the IAR Embedded Workbench IDE for Arm. Using existing project. Did not see the SDK component manager so I just added the required files to the existing utilities. It built with no errors. Is this correct? Also will this debug console and shell show up on one of the USB ports?

0 件の賞賛
返信

1,123件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @DanielTC,

Adding the components manually would be the option to do so on IAR, yes. If there were no build errors, then it should work and show up on one of the COM ports, as you mention.

BR,
Edwin.

0 件の賞賛
返信