RT1176 debug console and shell

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 debug console and shell

1,194 Views
DanielTC
Contributor I

Under SBR\SDK_2_15_100_MIMXRT1170-EVK\devices\MIMXRT1176\utilities

How do you build the debug console and shell?

Or can you add the utilities directory to an existing project?

0 Kudos
Reply
3 Replies

1,167 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @DanielTC,

You can add these utility components when creating a new project on the components section:

EdwinHz_0-1718297927173.png

Or for an existing project, you can open the SDK component manager window and select them there:

EdwinHz_1-1718297966297.png

EdwinHz_2-1718297973035.png

BR,
Edwin.

 

0 Kudos
Reply

1,137 Views
DanielTC
Contributor I

I'm using the IAR Embedded Workbench IDE for Arm. Using existing project. Did not see the SDK component manager so I just added the required files to the existing utilities. It built with no errors. Is this correct? Also will this debug console and shell show up on one of the USB ports?

0 Kudos
Reply

1,112 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @DanielTC,

Adding the components manually would be the option to do so on IAR, yes. If there were no build errors, then it should work and show up on one of the COM ports, as you mention.

BR,
Edwin.

0 Kudos
Reply