Quirk to watch for in SDK 2.5.0 for LPC804 in fsl_gpio.c GPIO_PortInit()

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quirk to watch for in SDK 2.5.0 for LPC804 in fsl_gpio.c GPIO_PortInit()

636 Views
mike_katz
Contributor I

In version 2.1.1 the GPIO_PortInit code is:

void GPIO_PortInit(GPIO_Type *base, uint32_t port)
{
#if !(defined(FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL) && FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL)
    assert(port < ARRAY_SIZE(s_gpioClockName));

    /* Upgate the GPIO clock */
    CLOCK_EnableClock(s_gpioClockName[port]);
#endif /* FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL */
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

In 2.1.2 it has changed to:

void GPIO_PortInit(GPIO_Type *base, uint32_t port)
{
#if !(defined(FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL) && FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL)
    assert(port < ARRAY_SIZE(s_gpioClockName));

    /* Upgate the GPIO clock */
    CLOCK_EnableClock(s_gpioClockName[port]);
#endif /* FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL */
#if !(defined(FSL_FEATURE_GPIO_HAS_NO_RESET) && FSL_FEATURE_GPIO_HAS_NO_RESET)
    /* Reset the GPIO module */
    RESET_PeripheralReset(s_gpioResets[port]);
#endif
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

The code from line 9 through line 12 is new.  In version 2.1.1 GPIO_PortInit() could be called more than once for a given port without affecting the configuration of that port.  However, version 2.1.2, if your processor supports port reset, resets the ports configuration.  So if this is called a 2nd time, any configuration done prior to 2nd call will reset the prior configuration.

For example:

    gpio_pin_config_t gpio_config =
    {
        kGPIO_DigitalOutput, 0,
    };

    //
    //  initialize output GPIOs
    //
    GPIO_PortInit(BOARD_INITPINS_HeartBeat_LED_GPIO, BOARD_INITPINS_HeartBeat_LED_PORT);
    GPIO_PinInit(BOARD_INITPINS_HeartBeat_LED_GPIO, BOARD_INITPINS_HeartBeat_LED_PORT, BOARD_INITPINS_HeartBeat_LED_PIN, &gpio_config);
    GPIO_PinInit(BOARD_INITPINS_DebugLed1_GPIO, BOARD_INITPINS_DebugLed1_PORT, BOARD_INITPINS_DebugLed1_PIN, &gpio_config);
    GPIO_PinInit(BOARD_INITPINS_ChargerDisable_GPIO, BOARD_INITPINS_ChargerDisable_PORT, BOARD_INITPINS_ChargerDisable_PIN, &gpio_config);

    //
    //  Initialize the input GPIOs
    //
    gpio_config.pinDirection = kGPIO_DigitalInput;
    GPIO_PortInit(BOARD_INITPINS_HeartBeat_LED_GPIO, BOARD_INITPINS_HeartBeat_LED_PORT);
    GPIO_PinInit(BOARD_INITPINS_Charging_GPIO, BOARD_INITPINS_Charging_PORT, BOARD_INITPINS_Charging_PIN, &gpio_config);
    GPIO_PinInit(BOARD_INITPINS_LeftRightSelect_GPIO, BOARD_INITPINS_LeftRightSelect_PORT, BOARD_INITPINS_LeftRightSelect_PIN, &gpio_config);
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

The call to GPIO_PortInit() on line 18 may, depending on your processor capabilities, reset the pin initialization done on lines 10 -> 12.

If your code only calls GPIO_PortInit() once then you are ok:

    gpio_pin_config_t gpio_config =
    {
        kGPIO_DigitalOutput, 0,
    };

    //
    //  initialize output GPIOs
    //
    GPIO_PortInit(BOARD_INITPINS_HeartBeat_LED_GPIO, BOARD_INITPINS_HeartBeat_LED_PORT);
    GPIO_PinInit(BOARD_INITPINS_HeartBeat_LED_GPIO, BOARD_INITPINS_HeartBeat_LED_PORT, BOARD_INITPINS_HeartBeat_LED_PIN, &gpio_config);
    GPIO_PinInit(BOARD_INITPINS_DebugLed1_GPIO, BOARD_INITPINS_DebugLed1_PORT, BOARD_INITPINS_DebugLed1_PIN, &gpio_config);
    GPIO_PinInit(BOARD_INITPINS_ChargerDisable_GPIO, BOARD_INITPINS_ChargerDisable_PORT, BOARD_INITPINS_ChargerDisable_PIN, &gpio_config);

    //
    //  Initialize the input GPIOs
    //
    gpio_config.pinDirection = kGPIO_DigitalInput;
    GPIO_PinInit(BOARD_INITPINS_Charging_GPIO, BOARD_INITPINS_Charging_PORT, BOARD_INITPINS_Charging_PIN, &gpio_config);
    GPIO_PinInit(BOARD_INITPINS_LeftRightSelect_GPIO, BOARD_INITPINS_LeftRightSelect_PORT, BOARD_INITPINS_LeftRightSelect_PIN, &gpio_config);
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Just another slight code change in an SDK that can break an existing application.

0 Kudos
1 Reply

515 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mike Katz,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Thanks for your sharing.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos