Question of the "flexcan_pretended_networking_wakeup" about frdmmcxn236

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question of the "flexcan_pretended_networking_wakeup" about frdmmcxn236

319件の閲覧回数
yhc123
Contributor II

I'm looking the "flexcan_pretended_networking_wakeup" case of SDK_25_03_00_FRDM-MCXN236, and I want to know what's the meaning of wake up payload range in the readme file, 0x0055000000000000 seems like a 64bit data but the platfporm just 32bits.

yhc123_1-1750164307603.png

 

Does the payload for sending data need to be between 0x00550000000000 and 0x005600000000000 for the receiving end to receive it? Why receiving end can reveive the match message 2 and  match message 1, they are out of range maybe.

yhc123_0-1750164281288.png

 

0 件の賞賛
返信
1 返信

280件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @yhc123,

The wake-up payload range is set as an example of how to define a range for the pretended device to be woken up. However, this is only an illustrative method, as it is not actually used on the wakeup procedure. In the example, as long as 4 messages are received, the device will wake-up.

BR,
Edwin.

0 件の賞賛
返信