Question about removal of three-slot mode for Encrypted XIP in MCUboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about removal of three-slot mode for Encrypted XIP in MCUboot

47 Views
mastupristi
Senior Contributor I

Hello,

while testing the MCUboot fork from NXP, I noticed that in the September preview release a useful feature has been removed.
Specifically, I am referring to the support for three-slot mode with Encrypted XIP (two staging slots + one execution slot, used to enable revert).

I saw this commit:
7c455cf2d 

with the message:

[MCUX-80671] Encrypted XIP: remove customization for three slot mode

 

Could you please explain why this functionality was removed?

  • Is it considered deprecated or no longer supported?
  • Are there plans to reintroduce it, or should we adapt our designs to use only two slots in case of encrypted XIP?
  • Was this related to technical limitations, or more to simplify the codebase?

This feature was quite valuable for our use case, and understanding the rationale behind its removal will help us plan the next steps.

Thank you in advance for your clarification.

 

best regards

Max

Tags (2)
0 Kudos
Reply
2 Replies

35 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @mastupristi,

I will investigate this topic internally. Could you please provide the MCU that you are currently using?

 

0 Kudos
Reply

18 Views
mastupristi
Senior Contributor I

Hi @EdwinHz 

i'm using RT1021

 

regards

Max

0 Kudos
Reply