Print Failed Console in MCUXpresso SDK RT1050-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Print Failed Console in MCUXpresso SDK RT1050-EVK

Jump to solution
1,050 Views
rubensjunior
Contributor IV

Dear friends,

I am developing a project whit the MIMXRT1052. For the initial tests, I am using the SDK for MCUXpresso. I am testing the example evkbimxrt1050_semc. This example is running normaly, but the console isn’t print the text of the debbug. When I create a simple project, as a Hello Word, the console print normaly, but when I use the SDK example, the console no print. Please, I need your help.

PS.: I am using the QSPI Flash (I altered the resistors for the selection). The my QSPI Flash is the IS25LP128. 

Best Regards.

Rubens Júnior

Labels (1)
1 Solution
909 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Rubens Junior

Could you confirm that you have the example code set with the semihosting enabled? you can go to the Quick settings>>SDK Debug Console>>Semihost Console:

pastedImage_1.png

Best regards
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

View solution in original post

2 Replies
910 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Rubens Junior

Could you confirm that you have the example code set with the semihosting enabled? you can go to the Quick settings>>SDK Debug Console>>Semihost Console:

pastedImage_1.png

Best regards
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

909 Views
rubensjunior
Contributor IV

Dear Jorge,

Thankyou very much! It's correct.

Best Regards,

Rubens Júnior

0 Kudos