Port latest version of lwIP 2.1.0 with MCUXpressoSDK 2.5.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port latest version of lwIP 2.1.0 with MCUXpressoSDK 2.5.0

1,178 Views
saad_saeed
Contributor III

Hello,

I am using MCUXpresso IDE v10.3.0, I have downloaded the latest MCUXpressoSDK 2.5.0. The lwIP version in the latest SDK is 2.0.3 which does not support DHCPv6. The latest stable version which supports DHCPv6 is lwIP v2.1.0.

KIndly, tell me how should I port this or can you provide me the latest MCUXpressoSDK ported with lwIP v2.1.0?

Thanks,

Saad,. 

Tags (2)
0 Kudos
Reply
1 Reply

869 Views
miduo
NXP Employee
NXP Employee

Hello,

I saw a duplicate thread: https://community.nxp.com/thread/493052 and that thread had been processed already. Please follow that thread. Thanks.

0 Kudos
Reply