Hello Amer,
I attached it for you.
You can also download SDK package and Docs from: https://mcuxpresso.nxp.com/en/select
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi NXP,
I'm using the latest MCUXpresso 11.3.0.
I installed the SDK_2.9.0_FRDM-K64F for which I'd like to access to the API documentation.
I read the above answer, but it doesn't solve the issue.
I can open the SDK Getting started or the Release notes from:
Unfortunately none of the 2 point me to the SDK documentation. I found it just using Google a this address but of course I think there is a better way to access to the official documentation. What is it?
One more, I think that would be very appreciated been able to open the SDK html (exist?!?) from within the MCUXpresso IDE.
Would be also very useful use the context menu over a function to open directly the function doc (I suppose the SDK is done with the Doxygen).
Many thanks!
Kind regards,
AGA
Hello Amer Naseem,
You can find it under SDK package->docs after you download SDK.
Or you can tell me which chip you use, I will send it for you.
Hope it helps,
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Amer,
I attached it for you.
You can also download SDK package and Docs from: https://mcuxpresso.nxp.com/en/select
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------