New LPC54S018JxM project requires fsl_emc and fsl_debug_console

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

New LPC54S018JxM project requires fsl_emc and fsl_debug_console

ソリューションへジャンプ
2,299件の閲覧回数
rex_lam
Contributor IV

When I create a new LPC54S018JxM project, the SDK wizard tool requires emc and debug_console to be selected. When I deselect the emc driver or debug_console utility, I get this error.

"Unsatisfied component 'lpcxpresso54s018m' dependencies!
The following dependencies are missing: '[debug_console_lite(UTILITIES), emc(DRIVER)]'

The SDK wizard will not allow me to finish creating the project without these two components even though my project does not use them, and I can build fine without them. Why are these two dependencies required?

0 件の賞賛
返信
1 解決策
2,251件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rex_lam,

This is because when create new project we choose based on LPCxpresso54s018M board.

If you just based on  CHIP LPC54S018JxM, no need choose them:

Alice_Yang_0-1621935145260.png

Alice_Yang_1-1621935402909.png

 

Or if enable board, then choose "empty board files" also can work.

Alice_Yang_2-1621935669480.png

 

BR

Alice

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,285件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rex_lam,

Do you use MCUXpresso IDE? Could you please attach your project and take a screenshot show your selection. thanks.

 

BR

Alice

0 件の賞賛
返信
2,272件の閲覧回数
rex_lam
Contributor IV

Yes, I use MCUXpresso IDE. I apologize, as I realize I have posted the question in the SDK forum instead of the IDE forum.

I have attached a sample project.

Here is the screenshot when emc is deselected.

rex_lam_0-1621613905782.png

Here is the screenshot when debug_console is deselected.

rex_lam_1-1621613995996.png

 

0 件の賞賛
返信
2,252件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rex_lam,

This is because when create new project we choose based on LPCxpresso54s018M board.

If you just based on  CHIP LPC54S018JxM, no need choose them:

Alice_Yang_0-1621935145260.png

Alice_Yang_1-1621935402909.png

 

Or if enable board, then choose "empty board files" also can work.

Alice_Yang_2-1621935669480.png

 

BR

Alice

 

 

0 件の賞賛
返信
2,243件の閲覧回数
rex_lam
Contributor IV

Thank you for your help. Much appreciated.

0 件の賞賛
返信