Using MCUXpresso IDE, I have cloned a few 2.3.1 SDK examples for the FRDM-K22F eval board.
I then created the <peripheral, clock_config, pin_mux>.<c,h> files using MCUXpresso Config for the FRDM-K22F eval board.
The SDK pin_mux.c file has YAML comments, as do the files generated by MCUXpresso Config.
However, the SDK pin_mux.c file seems to be an example minimal version of the Config pin_mux.c.
The SDK files board.<c,h> are the equivalent to peripheral.<c,h> in Config.
main() in an SDK example calls
BOARD_InitPins();
BOARD_BootClockHSRUN();
BOARD_InitDebugConsole();
Using the Config files it appears that main() should call
BOARD_InitBootPins();
BOARD_BootClockHSRUN();
BOARD_InitBootPeripherals(); // BOARD_InitDEBUG_UARTPeripheral() called.
My goal is to be able to configure all the peripherals I need for a target K22 project. The SDK examples configure only one peripheral per example. My project will need to have multiple peripherals, ADC, GPIO, etc. configured at boot.
I believe I could substitute the files from Config for the board/pin_mux/clock_config files in the SDK and call the appropriate functions in main().
Is this an expected method to customize an SDK example?