Hello,
I am running the flexcan_interupt example program from the FRDM-KW36 Dev. Board on the MKW36A512VFP4 Controller.
When I ran the example with a baud rate of 125k I can send and receive Messages with out any problems. But when I change the baud rate to 100k, 250k ,500k or 1000k I can't get the program to work. With these baud rates as sonn as there is traffic on the CAN bus the flexcan_callback function reports an error 5310.
With the baud rate of 125k I can monitor the CAN messages with a Scope. But with all other baud rates the Scope can't decode the message.
Do I have to change some clock or bit timing settings to get the other baud rates to work?
What confuses me the most is that the flexcan_interupt example is configured with a baud rate of 1000k an it doesn't work.
Any help is highly appreciated.
Regards,
Lukas
解決済! 解決策の投稿を見る。
Hello,
Could you please help me checking this thread and confirm if this helps you ?
https://community.nxp.com/docs/DOC-341824
I believe that you can find there the information you are looking for.
Regards,
Estephania
Hello,
Could you please help me checking this thread and confirm if this helps you ?
https://community.nxp.com/docs/DOC-341824
I believe that you can find there the information you are looking for.
Regards,
Estephania
Hello Estephania,
thanks for the help. That was exactly what I was looking for.
Regards,
Lukas