MIMXRT1061xxxxB part support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1061xxxxB part support

ソリューションへジャンプ
2,324件の閲覧回数
astrobuf
Contributor I

In SDK builder, the part support for MIMXRT1061xxxxB variants is incomplete. Is there somewhere else to look?

SDK MIMXRT1061xxxxB.png

0 件の賞賛
返信
1 解決策
2,293件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @astrobuf ,

    You totally can use the A part code, take an example, as you know, the NXP MIMXRT1060-EVK board is the MIMXRT1062DVL6B, but if you check the related SDK project, you will find it also the A part.

kerryzhou_0-1659426392902.png

Until now, I didn't find any issues.

About the A and B part difference, just check the errata document.

 

Wish it helps you!

Best Regards,

Kerry

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,301件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @astrobuf ,

   You are right, that is not the complete partnumber.

   Which detail MIMXRT1062xxxB part you want to use?

  The following part?

MIMXRT1061DVL6B
 MIMXRT1061DVJ6B

  If yes, I think you also can generate the A part,:

kerryzhou_0-1659361076961.png

That software also can be used in the B part.

 

Wish it helps you!

Best Regards,

kerry

 

0 件の賞賛
返信
2,299件の閲覧回数
astrobuf
Contributor I

We want to use MIMXRT1061DVJ6B.  Already setup the project with the A part, but was not sure if there were some differences. If they are the same, we are all good.

Thanks.

Peter

 

0 件の賞賛
返信
2,294件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @astrobuf ,

    You totally can use the A part code, take an example, as you know, the NXP MIMXRT1060-EVK board is the MIMXRT1062DVL6B, but if you check the related SDK project, you will find it also the A part.

kerryzhou_0-1659426392902.png

Until now, I didn't find any issues.

About the A and B part difference, just check the errata document.

 

Wish it helps you!

Best Regards,

Kerry

 

0 件の賞賛
返信