MIMRT106x SNVS Low-Power Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMRT106x SNVS Low-Power Mode

ソリューションへジャンプ
1,591件の閲覧回数
jeffthompson
Contributor V

I’m working on low-power mode and wakeup and have read application note “AN12245—Power Consumption and Measurement of i.MX RT1060”, along with the “MCUXpresso SDK Reference Manual_MIMXRT1060”, but I don't see where either explains how to put the MCU into low-power SNVS mode.

Also, I'm assuming that setting GPIO5, pin 0, as an interrupt (rising edge for my hardware) is sufficient for waking up the processor to run in Full-Speed Run mode. Is that the case?

I'm using MCUXpresso 11.01 for the MIMXRT1062DVJ6A, and MCUXpresso SDK USB Stack, Rev. 10, 06/2019.

タグ(2)
1 解決策
1,473件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One can find the detail information for the question as the link https://www.nxp.com/docs/en/application-note/AN12085.pdf . Hope it help you.Have a nice day.

元の投稿で解決策を見る

1 返信
1,474件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One can find the detail information for the question as the link https://www.nxp.com/docs/en/application-note/AN12085.pdf . Hope it help you.Have a nice day.